License of FreeRTOS for i.MX7D

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

License of FreeRTOS for i.MX7D

Jump to solution
917 Views
ko-hey
Senior Contributor II

Hi all

Let me confirm about the licensing of FreeRTOS for i.MX7D.

I plan to do some tests with FreeRTOS in MCIMX7SABRE and downloaded the FreeRTOS from following link.

FreeRTOS_iMX7D_1.0.1_WIN 

I got following two files for licensing when I installed it.

LA_OPT_Base_License.htm
SW-Content-Register-FreeRTOS-BSP-1.0.1-i.MX7D.txt

Does the license of SW-Content-Register-FreeRTOS-BSP-1.0.1-i.MX7D.txt include the license of LA_OPT_Base_License.htm ?

For example,

Does the license of FreeRTOS BSP Peripheral Driver follow the license of LA_OPT_Base_License.htm ?

Ko-hey

Labels (1)
0 Kudos
1 Solution
733 Views
art
NXP Employee
NXP Employee

Q. Which license version should user check ?

A. Of course, the latest v17 license version should be checked.

Q. Can I treat it as a BSD-3-Clause?

A. Yes.

Best Regards,

Artur

View solution in original post

0 Kudos
6 Replies
733 Views
art
NXP Employee
NXP Employee

SW-Content-Register-FreeRTOS-BSP-1.0.1-i.MX7D.txt is not the license, but the BSP package content description. All package content, described in SW-Content-Register-FreeRTOS-BSP-1.0.1-i.MX7D.txt, is covered by the licensing rules, described in LA_OPT_Base_License.htm .


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
733 Views
ko-hey
Senior Contributor II

Artur

Thank you!

Ko-hey

0 Kudos
733 Views
ko-hey
Senior Contributor II

Hi Artur

I have another question. could you tell the following question ?

Q1.

Which license version should user check ?


In the license "LA_OPT_BASE_LICENSE v17 December 2016" displayed on the download screen, there is a FreeRTOS indication on APPENDIX A.
However, there is no entry in the file "LA_OPT_BASE_LICENSE v17 December 2016" that can be created in the installed folder.
We compared the license and found there are description for FreeRTOS in "LA_OPT_BASE_LICENSE v17 December 2016" displayed on the download screen.


Which license version should user check ?

Q2.

In APPENDIX A of [LA_OPT_BASE_LICENSE v 17 December 2016, there is no mention of CMSIS DSP Library, CMSIS Core header files, FreeRTOS BSP Peripheral Driver and OpenAMP.
it is not listed in the APPENDIX A list but any license is described in the BSD-3-Clause.

Can I treat it as a BSD-3-Clause? "

Ko-hey

0 Kudos
734 Views
art
NXP Employee
NXP Employee

Q. Which license version should user check ?

A. Of course, the latest v17 license version should be checked.

Q. Can I treat it as a BSD-3-Clause?

A. Yes.

Best Regards,

Artur

0 Kudos
733 Views
ko-hey
Senior Contributor II

Hi Artur

Could you follow and answer above question ?

Ko-hey

0 Kudos
733 Views
ko-hey
Senior Contributor II

Could someone follow and answer this thread ?

Ko-hey

0 Kudos