Libipu: file in wrong format

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Libipu: file in wrong format

797 次查看
christophe
Contributor V

Hi all,

When linking with libipu.so.0, this message occurs:

libipu.so.0: could not read symbols: File in wrong format

If ii create a dummy.so lib, i can link it perfectly, so it's probably libipu.so.0 that is different.

I notice a compilator difference when using the file command:

lucid@ubuntu:~/rainbow$ file dummy.so
bidon.so: ELF 32-bit LSB shared object, Intel 80386, version 1 (SYSV), dynamically linked, not stripped

and

lucid@ubuntu:~/rainbow$ file libipu.so.0
libipu.so.0: ELF 32-bit LSB shared object, ARM, version 1 (SYSV), dynamically linked, not stripped

libipu.so.0 is compilated with ARM version, so i suppose i've to compile too with ARM. How can i configure makefile to use ARM compilator ?

thanks.

标签 (1)
0 项奖励
回复
0 回复数