Hi community.
Our customer has question below.
To ask about the leak voltage to USB_OTG_DP / N during the reset.
Please see atached Fig.
Currently, leak voltage will have occurred from the outside, on the system (actual device) USB_OTG_DP / N.
Leak voltage is about 0.3V, but we are concerned about the latch-up and reverse current flow occurs because it has been applied to the PowerSpurce (USB_OTG_VBUS and VDDUSB_CAP) before the launch of the USB_OTG_DP / N.
Would you please advice to me, Is it necessary for the latch-up and the current back-flow measures or accepable range .
Thasnks,
Best.
T.Takahashi
Solved! Go to Solution.
Hi Takashi
this is smal voltage should not cause problems, also
it is less then Vil from Table 7-7 USB 2.0 specification.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Takashi
this is smal voltage should not cause problems, also
it is less then Vil from Table 7-7 USB 2.0 specification.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------