Layout guide line for uSDHC with SDR104 mode in i.MX6

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Layout guide line for uSDHC with SDR104 mode in i.MX6

Jump to solution
3,489 Views
keitanagashima
Senior Contributor I

Dear Sir or Madam,

Hello.

My customer would like to use the uSDHC interface with SDR-104 mode.

This mode is very fast speed (104 MB/s max).

Do you have Layout guide line for uSDHC with SDR104 mode in i.MX6?

BR,

Keita

Labels (5)
0 Kudos
Reply
1 Solution
2,749 Views
igorpadykov
NXP Employee
NXP Employee

Hi Keita

i.MX6 User Guide does not provide special recommendations

for SDR-104 mode layout. However one can use sect.

3.12 Impedance signal recommendations IMX6DQ6SDLHDG and

sect.6 SD/MMC/SDIO Card AN4215 i.MX28 Layout Guidelines

(given also for double data rate mode).

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
3 Replies
2,750 Views
igorpadykov
NXP Employee
NXP Employee

Hi Keita

i.MX6 User Guide does not provide special recommendations

for SDR-104 mode layout. However one can use sect.

3.12 Impedance signal recommendations IMX6DQ6SDLHDG and

sect.6 SD/MMC/SDIO Card AN4215 i.MX28 Layout Guidelines

(given also for double data rate mode).

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply
2,749 Views
keitanagashima
Senior Contributor I

Hi Igor,

Thank you for your reply.

I found the below description on HW Design Checking List for i.MX6DQSDL

"50Ω impedance control"

"Match Clock and Data signals  ± 50 mils"

Is it possible to reference above descriptions, too?

Best Regards,

Keita

0 Kudos
Reply
2,749 Views
igorpadykov
NXP Employee
NXP Employee

Hi Keita

yes one can also use this document too, as

"summary based on IMX6DQ6SDLHDG and our supporting experience"

Best regards

igor

0 Kudos
Reply