All,
Can someone please list the latest versions of Ubuntu and/or Fedora
that are guaranteed/known to work with LTIB 9.1.1 on i.MX53 at least?
So far I am having LTIB fail on Ubuntu 11.10.
I ran:
./ltib -m config
All the following build OK:
Processing: rpm-fs
Processing: fake-provide
Processing: mkspooflinks
Processing: distcc
Processing: ccache
Processing: bison
Processing: flex
Processing: texinfo
Processing: autoconf
Processing: libtool
...
LTIB breaks at lkc with this error:
...
Processing: lkc
=================
....
util.c:(.text+0xa58): undefined reference to `winch'
util.c:(.text+0xa6c): undefined reference to `waddch'
util.c:(.text+0xa8b): undefined reference to `wnoutrefresh'
collect2: ld returned 1 exit status
make: *** [mconf] Error 1
error: Bad exit status from /opt/freescale/ltib/tmp/rpm-tmp.33058 (%build)
RPM build errors:
Bad exit status from /opt/freescale/ltib/tmp/rpm-tmp.33058 (%build)
Build time for lkc: 2 seconds
Failed building lkc
Died at ./ltib line 1380.
traceback:
main::build_host_rpms:1380
main::host_checks:1435
main:542
-------------------------------------------------------------------------------------------------------
I read somwere that it might be because of ncurses.
I installed "libncursesw5-dev" which was picked instead of "libncurses-dev"
and "ncurses-dev" which I tried.
Any clues what I am missing?
"/opt/freescale/ltib/tmp/rpm-tmp.33058" is attached:
Thanks,
Ad.
----------------------------
Original Attachment has been moved to: 515-optfreescaleltibtmprpmtmp.33058