Latest linux image for imx6

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Latest linux image for imx6

ソリューションへジャンプ
1,879件の閲覧回数
eugenephua
Contributor III

Hi there, i am using the imx6 Sabre Smart Devices Board. I saw there is a new linux binary demo file at : http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=RDIMX6SABREBRD&fpsp=1&tab=Design_Tool... -> L3.10.53_1.1.0_iMX6QDLS_Bundle. I followed the manual i.MX Linux User's Guide 4.3.2 Copying the Full SD card image. However, when i try booting the board, it does not boot up...

This is the serial output:

U-Boot 2014.04 (Jan 05 2015 - 13:20:35)

CPU:   Freescale i.MX6Q rev1.2 at 792 MHz

CPU:   Temperature 41 C, calibration data: 0x5c14ef7d

Reset cause: POR

Board: MX6-SabreSD

I2C:   ready

DRAM:  1 GiB

MMC:   FSL_SDHC: 0, FSL_SDHC: 1, FSL_SDHC: 2

MMC: no card present

MMC init failed

Using default environment

No panel detected: default to Hannstar-XGA

Display: Hannstar-XGA (1024x768)

In:    serial

Out:   serial

Err:   serial

Found PFUZE100 deviceid=10,revid=11

MMC: no card present

mmc1(part 0) is current device

Net:   FEC [PRIME]

Normal Boot

Hit any key to stop autoboot:  0

MMC: no card present

mmc1(part 0) is current device

MMC: no card present

Booting from net ...

FEC Waiting for PHY auto negotiation to complete......... TIMEOUT !

BOOTP broadcast 1

BOOTP broadcast 2

ラベル(3)
0 件の賞賛
返信
1 解決策
1,254件の閲覧回数
eugenephua
Contributor III

Ahhh... The SD card reader on the board was not good... After plugging in and out a few times finally it booted!!! :smileyshocked:

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,255件の閲覧回数
eugenephua
Contributor III

Ahhh... The SD card reader on the board was not good... After plugging in and out a few times finally it booted!!! :smileyshocked:

0 件の賞賛
返信
1,254件の閲覧回数
eugenephua
Contributor III

This is the printenv from u-boot:

baudrate=115200

boot_fdt=try

bootcmd=mmc dev ${mmcdev};if mmc rescan; then if run loadbootscript; then run bootscript; else if run loadimage; then run mmcboot; else run netboot; fi; fi; else run netboot; fi

bootcmd_mfg=run mfgtool_args;bootz ${loadaddr} ${initrd_addr} ${fdt_addr};

bootdelay=1

bootscript=echo Running bootscript from mmc ...; source

console=ttymxc0

ethact=FEC

ethaddr=00:04:9f:02:6d:30

ethprime=FEC

fdt_addr=0x18000000

fdt_file=imx6q-sabresd.dtb

fdt_high=0xffffffff

image=zImage

initrd_addr=0x12C00000

initrd_high=0xffffffff

ip_dyn=yes

loadaddr=0x12000000

loadbootscript=fatload mmc ${mmcdev}:${mmcpart} ${loadaddr} ${script};

loadfdt=fatload mmc ${mmcdev}:${mmcpart} ${fdt_addr} ${fdt_file}

loadimage=fatload mmc ${mmcdev}:${mmcpart} ${loadaddr} ${image}

mfgtool_args=setenv bootargs console=ttymxc0,115200 rdinit=/linuxrc g_mass_storage.stall=0 g_mass_storage.removable=1 g_mass_storage.idVendor=0x066F g_mass_storage.idProduct=0x37FF g_mass_storage.iSerialNumber="" enable_wait_mode=off

mmcargs=setenv bootargs console=${console},${baudrate} ${smp} root=${mmcroot}

mmcautodetect=yes

mmcboot=echo Booting from mmc ...; run mmcargs; if test ${boot_fdt} = yes || test ${boot_fdt} = try; then if run loadfdt; then bootz ${loadaddr} - ${fdt_addr}; else if test ${boot_fdt} = try; then bootz; else echo WARN: Cannot load the DT; fi; fi; else bootz; fi;

mmcdev=1

mmcpart=1

mmcroot=/dev/mmcblk2p2 rootwait rw

netargs=setenv bootargs console=${console},${baudrate} ${smp} root=/dev/nfs ip=dhcp nfsroot=${serverip}:${nfsroot},v3,tcp

netboot=echo Booting from net ...; run netargs; if test ${ip_dyn} = yes; then setenv get_cmd dhcp; else setenv get_cmd tftp; fi; ${get_cmd} ${image}; if test ${boot_fdt} = yes || test ${boot_fdt} = try; then if ${get_cmd} ${fdt_addr} ${fdt_file}; then bootz ${loadaddr} - ${fdt_addr}; else if test ${boot_fdt} = try; then bootz; else echo WARN: Cannot load the DT; fi; fi; else bootz; fi;

script=boot.scr

update_sd_firmware=if test ${ip_dyn} = yes; then setenv get_cmd dhcp; else setenv get_cmd tftp; fi; if mmc dev ${mmcdev}; then if ${get_cmd} ${update_sd_firmware_filename}; then setexpr fw_sz ${filesize} / 0x200; setexpr fw_sz ${fw_sz} + 1; mmc write ${loadaddr} 0x2 ${fw_sz}; fi; fi

0 件の賞賛
返信