Latest libGAL and friends

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Latest libGAL and friends

634件の閲覧回数
natesigrist
Contributor III

Is the only source for the iMX6 GPU in the Yocto project?

 -> downloads.yoctoproject.org/mirror/sources/imx-gpu-viv-5.0.11.p8.3-hfp.bin

 

Is there an up-to-date version somewhere?  This was from 2016 >< and have long since expired since the xserver uses new ABIs and such.

Here is a reference to the work I've done in so far in implementing the proprietary binaries,

Installing libGL and friends for Linux 4.9 

ラベル(5)
タグ(3)
0 件の賞賛
1 返信

481件の閲覧回数
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hi Nate,

The latest version is 5.0.11p8.6. Will have new version when k4.9.88 comes up.

0 件の賞賛