Latest libGAL and friends

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Latest libGAL and friends

2,115 Views
natesigrist
Contributor III

Is the only source for the iMX6 GPU in the Yocto project?

 -> downloads.yoctoproject.org/mirror/sources/imx-gpu-viv-5.0.11.p8.3-hfp.bin

Is there an up-to-date version somewhere?  This was from 2016 >< and have long since expired since the xserver uses new ABIs and such.

Tags (4)
0 Kudos
Reply
4 Replies

1,707 Views
natesigrist
Contributor III

Here is a reference to the work I've done in so far in implementing the proprietary binaries,

https://community.nxp.com/thread/477594 

0 Kudos
Reply

1,707 Views
igorpadykov
NXP Employee
NXP Employee

Hi Nate

one can look at latest Linux 4.9.88_2.0.0 BSP, use Yocto Guide for bilding:

https://www.nxp.com/webapp/Download?colCode=L4.9.88_2.0.0_LINUX_DOCS&Parent_nodeId=13376994810717061... 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,707 Views
natesigrist
Contributor III

Also, why is this assumed answered?!

0 Kudos
Reply

1,707 Views
natesigrist
Contributor III

igorpadykov‌ Thanks for the documentation :-)  However, my question was about the most recent location to find these binaries.  Obviously, Preferably source code...  So where might I find these library files???

0 Kudos
Reply