LXC docker

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
5,322件の閲覧回数
niklasmolin
Senior Contributor I

Hi.

I wonder if anyone has added docker (using LXC)?

Thanks,

Niklas

ラベル(3)
タグ(2)
0 件の賞賛
1 解決策
2,023件の閲覧回数
niklasmolin
Senior Contributor I

We have docker 0.10 working in our i.MX6 now.

Using the following link when I compile (so far it's on the target board) github.com/archlinuxarm/PKGBUILDs/tree/master/community/docker

Remember to include libc.a and libpthread.a in your image, since docker is statically including this libraries.

You also need to add a couple of things in the kernel (menuconfig), but I'll include this list later plus I also added a few things in local.conf.

We had more luck to use lxc instead of libcontainer (docker -d -e lxc)

元の投稿で解決策を見る

0 件の賞賛
11 返答(返信)
2,023件の閲覧回数
niklasmolin
Senior Contributor I

I managed to get docker to start up now.

So far I haven't had time to see if I can create a docker container yet (will try that either today or later this week).

But when I start docker it looks promising:

[/var/lib/docker|1318a470] +job serveapi(unix:///var/run/docker.sock)

[/var/lib/docker|1318a470] +job initserver()

[/var/lib/docker|1318a470.initserver()] Creating server

2014/04/17 23:05:32 Listening for HTTP on unix (/var/run/docker.sock)

bio: create slab <bio-1> at 1

device-mapper: thin: Data device (loop0) discard unsupported: Disabling discard passdown.

[/var/lib/docker|1318a470] +job init_networkdriver()

[/var/lib/docker|1318a470.init_networkdriver()] creating new bridge for docker0

[/var/lib/docker|1318a470.init_networkdriver()] getting iface addr

[/var/lib/docker|1318a470] -job init_networkdriver() = OK (0)

2014/04/17 23:05:34 WARNING: cgroup mountpoint not found for memory

Loading containers: : done.

[/var/lib/docker|1318a470.initserver()] Creating pidfile

[/var/lib/docker|1318a470.initserver()] Setting up signal traps

[/var/lib/docker|1318a470] -job initserver() = OK (0)

[/var/lib/docker|1318a470] +job acceptconnections()

[/var/lib/docker|1318a470] -job acceptconnections() = OK (0)

When i have everything up an running, I'll write down the procedure I did you make it working.

0 件の賞賛
2,023件の閲覧回数
niklasmolin
Senior Contributor I

Right now I have a problem with cgroup:

container.go:788 Error running container: cgroup mountpoint not found for cpu

0 件の賞賛
2,024件の閲覧回数
niklasmolin
Senior Contributor I

We have docker 0.10 working in our i.MX6 now.

Using the following link when I compile (so far it's on the target board) github.com/archlinuxarm/PKGBUILDs/tree/master/community/docker

Remember to include libc.a and libpthread.a in your image, since docker is statically including this libraries.

You also need to add a couple of things in the kernel (menuconfig), but I'll include this list later plus I also added a few things in local.conf.

We had more luck to use lxc instead of libcontainer (docker -d -e lxc)

0 件の賞賛
419件の閲覧回数
sistlajr6
Contributor II

Hi Niklas,

I would like to check if you have had success with docker on IMX6, would be really nice if you could share the instructions for the same. 

0 件の賞賛
2,023件の閲覧回数
stevezilla
Contributor II

Niklas,

Have you had any success getting Docker running?  I'm interested in attempting this myself, would like to get any feedback about your efforts.  Thanks!

0 件の賞賛
2,023件の閲覧回数
niklasmolin
Senior Contributor I

After I managed to include the GO application, I managed to compile the docker (getting ideas from following link: Docker on Raspberry Pi).

Right now I'm trying to figure out how to enable the AUFS, since docker seems to be depending on this.

0 件の賞賛
2,023件の閲覧回数
tommanley
Contributor I

Thank you for trying to get this working. I think docker on i.MX would open up some interesting possibilities for testing and deployments.

What version of docker are you trying? According to the docs AUFS isn't required as of version 0.7

http://docs.docker.io/en/latest/installation/kernel/

0 件の賞賛
2,023件の閲覧回数
niklasmolin
Senior Contributor I

I managed to include the device-mapper.

But now it complains that it can "find' mkfs.ext4.

I have notice before that I can't use the mkfs command. it always complains that either .ext2 or .ext3 or .ext4 is missing.

So now is a good time to figure this thing out.

0 件の賞賛
2,023件の閲覧回数
niklasmolin
Senior Contributor I

Hi Thomas.

I'm trying with docker version 0.7.1., since I wanted to avoid the dependency on AUFS (which is not part of the i.mx kernel).

I had to do some patches in some file, for it to even be able to "compile/run" on a 32bit ARM (since it was limited to amd64).

Now I'm just trying to fix some other problems, which has to do with the device-mapper.

By the way, do you know if it's possible to add the device-mapper in the image?

This seems to be one problem, that I don't have /dev/mapper in my build.

For the moment I'm doing this on the side, since we don't need to have this working for some time.

But I'll update this when I have more progress.

/Niklas

0 件の賞賛
2,023件の閲覧回数
niklasmolin
Senior Contributor I

Has anyone managed to install Go programming tools for Freescale?

0 件の賞賛
2,023件の閲覧回数
niklasmolin
Senior Contributor I

I managed to install the Go.

Planning on create a recipe for this, so I don't have to manually install on the board.

0 件の賞賛