LVDS0 + LCD mode supoort

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LVDS0 + LCD mode supoort

967 Views
yuhundehao
Contributor III

my platform imx6q ,I think support lvds0 and lcd mode .

Lvds0 is used as the display screen, and LCD is connected to the computer display screen through the conversion of vaga chip

How  to do?

 
Labels (2)
0 Kudos
Reply
2 Replies

871 Views
igorpadykov
NXP Employee
NXP Employee

Hi yuhundehao

one can look at suggestions provided on

https://community.nxp.com/thread/307613 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

871 Views
mahi
Contributor IV

Please provide some more information.

Basically the only information you are giving is that you have an i.MX6Q.

What kind of platform do you have - something custom, a sabre board or any other evaluation board?

Are you running Linux(yocto), Android or Baremetal?

If Linux, which BSP - release or community?

If Android, which BSP, Version?

You want to connect a LCD module to your platform through LVDS? Yes this is possible, but for further assistance we need to know more about your project.

0 Kudos
Reply