LVDS display is not working in IMX custom board

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LVDS display is not working in IMX custom board

1,941件の閲覧回数
ashokp
Contributor I

Hi All,

 

I am using IMX6 based custom board and running kitkat from freescale. The kernel version is 3.0.35.

 

The HDMI and LCD displays are working fine  but LVDS display is not working fine. Please let me know if any issues in the code changes.

 

Below i copied the fb structure for your reference. Also attached my board file for your reference

 

static struct ipuv3_fb_platform_data sabresd_fb_data[] = {

        { /*fb0*/

        .disp_dev = "hdmi",

        .interface_pix_fmt = IPU_PIX_FMT_RGB24,

        .mode_str = "1920x1080M@60",

        .default_bpp = 24,

        .int_clk = false,

        .late_init = false,

        }, {

        .disp_dev = "lcd",

        .interface_pix_fmt = IPU_PIX_FMT_RGB24,

        .mode_str = "CLAA-WVGA",

        .default_bpp = 24,

        .int_clk = false,

        .late_init = false,

        }, {

        .disp_dev = "ldb",

        .interface_pix_fmt = IPU_PIX_FMT_RGB666,

//        .mode_str = "LDB-XGA",

        .default_bpp = 24,

        .int_clk = false,

        .late_init = false,

        },

};

 

 

 

static struct fsl_mxc_ldb_platform_data ldb_data = {

        .ipu_id = 0,   // ASHOK

        .disp_id = 0,

        .ext_ref = 1,

        .mode = LDB_SEP1,

        .sec_ipu_id = 0,

        .sec_disp_id = 0,

};

 

Thanks,

P.Ashok

Original Attachment has been moved to: board-mx6q_sabresd.c.zip

ラベル(3)
0 件の賞賛
返信
3 返答(返信)

1,297件の閲覧回数
alejandrolozan1
NXP Employee
NXP Employee

Hi,

I skimmed through the file and it seems to be fine.

I would start changing the IPU ids and see if there is any difference.

0 件の賞賛
返信

1,297件の閲覧回数
alejandrolozan1
NXP Employee
NXP Employee

Hi,

Have you tried with a different IPU id? Do you want the LVDS1 to be your primary display?

Regards,

Alejandro

0 件の賞賛
返信

1,297件の閲覧回数
ashokp
Contributor I

Hi Alejandro,

Yes i  want LVDS1 to be a primary display. Please let me know is anything wrong in my my board file

Thanks

P.Ashok

0 件の賞賛
返信