Dear Sir or Madam,
Hello.
My customer would like to connect i.MX6D and LVDS Display.
The LVDS display is 2 port I/F with (1920 x 720).
Can i.MX6D output odd / even number lines at the same time?
Refer to 39.5.1 Mapping of Input Data Busses in MCIMX6DQRM(Rev.1).
I consider Split Channel DI0 mode can use for above LVDS display.
Best Regards,
Keita
Solved! Go to Solution.
In Split mode , LVDS0 channel is odd pixels in line, LVDS1 channel is even pixels in line. so, add ldb=spl0 in your uboot parameters, then connect lvds0 to your odd pixel pins, connect lvds1 to your even pixel pins
Hi Keita,
kevinchan right,
Table 39-5 "Channel Mapping"
i.MX6DQ Reference Manual (rev.1 4/2013) shows that in split mode.
http://cache.freescale.com/files/32bit/doc/ref_manual/IMX6DQRM.pdf
Best regards
chip
In Split mode , LVDS0 channel is odd pixels in line, LVDS1 channel is even pixels in line. so, add ldb=spl0 in your uboot parameters, then connect lvds0 to your odd pixel pins, connect lvds1 to your even pixel pins