LVDS display configuration on MCIMX6Q5EYM10AD

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LVDS display configuration on MCIMX6Q5EYM10AD

875件の閲覧回数
Jack-Cha
Contributor V

Hi Champs

There's a question from Customer who wants to port LVDS panel on MCIMX6Q5EYM10AD.

The following is the panel timing specification. 

James_Arrow_0-1642398802538.png

The below dtsi is below to support their panel.

lvds-channel@0 {

fsl,data-mapping = "spwg";

fsl,data-width = <18>;

primary;

status = "okay";

display-timings {

native-mode = <&timing0>;

timing0: 800x480@60 {

clock-frequency = <25000000>;

hactive = <800>;

vactive = <480>;

hback-porch = <8>;

hfront-porch = <8>;

vback-porch = <8>;

vfront-porch = <8>;

hsync-len = <4>;

vsync-len = <4>;

};

};

};

 

According to their test observed, the video output clock runs 38MHz (pclk TCLK+, TCLK-) even though the clock set to 25MHz.

If clock speed sets up to 39MHz over, it runs normally. It always runs 38MHz when sets up under 39MHz. 

 

Please clarify the followings

1. iMX6' LVDS Minimum Resolution.

2. Guidance to support 800x480 (25MHz), or patch(code changes needed)

 

Thanks.

Regards, 

James

 

 

 

0 件の賞賛
返信
1 返信

868件の閲覧回数
joanxie
NXP TechSupport
NXP TechSupport

if you need to set lower resolution, you need change the clock parent, pls see this document:

https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/Porting-LVDS-LCD-With-Low-Resolution-to-...

0 件の賞賛
返信