LVDS_PHY_CTRL sharing

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LVDS_PHY_CTRL sharing

189 Views
krassimirestoya
Contributor III

Hi all,

We are trying to share access to LVDS_PHY_CTRL regster, owner by the A35 partition under Linux (Yocto). We want to access it via SCU board_ioctl or CM4 directly, if possible:

this is from board_ioctl:

        BRD_ERR(rm_set_peripheral_permissions(PWR_PT_6, SC_R_MIPI_0, SC_RM_PT_ALL, SC_RM_PERM_FULL)); // success
        BRD_ERR(rm_set_peripheral_permissions(PWR_PT_6, SC_R_MIPI_1, SC_RM_PT_ALL, SC_RM_PERM_FULL)); // success
        BRD_ERR(rm_set_peripheral_permissions(PWR_PT_6, SC_R_LVDS_0, SC_RM_PT_ALL, SC_RM_PERM_FULL)); // Fails with SC_ERR_PARM
        BRD_ERR(rm_set_peripheral_permissions(PWR_PT_6, SC_R_LVDS_1, SC_RM_PT_ALL, SC_RM_PERM_FULL)); // Fails with SC_ERR_PARM

 

        volatile int *p = (volatile int *)0x56221000; //LVDS_PHY_CTRL
        *p = 0;
        p = (volatile int *)0x56241000;
        *p = 0;

 

This code causes SCU to crash

 

0 Kudos
2 Replies

143 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

There are few hints that can help narrow this issue:

1. They suggestion is to ensure is to enabled power domain to access the register.

2. SC_ERR_PARM means bad parameter or combination of parameters

I am looking into SDK. I am working on getting to run example (dpu_blitblend) which controls register LVDS_PHY_CTRL from M4 core - Visteon's use-case. You have to try to extract specific setting needed.

But in the meantime, you  can see into example source code (attached) and use it as inspiration, what needs to be done to write the register.

Regards

0 Kudos

113 Views
krassimirestoya
Contributor III

Thanks for the reply, but we need to share it as the subject is

0 Kudos