LVDS Display output in I.MX8QM Board

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LVDS Display output in I.MX8QM Board

2,053件の閲覧回数
mallibeerala
Contributor III

Hi,

How can I enable LVDS Display output in I.MX8QM Board, which dtb file, I have to load for enabling LVDS display.

I am able to get HDMI display by following dtb file fsl-imx8qm-mek-hdmi.dtb

Thanks & Regards,
Mallikarjuna B.

 

 

ラベル(1)
0 件の賞賛
返信
4 返答(返信)

1,823件の閲覧回数
Sanjay_Pandey1
Contributor II

LVDS and MIPI Display is active by default in i.MX8QM MEY Evaluation Board. For HDMI you have to pass "hdmi" parameter while writing the image on board.  

I had tested it by through MIPI to HDMI and LVDS to HDMI converter.  

 

 

0 件の賞賛
返信

2,048件の閲覧回数
joanxie
NXP TechSupport
NXP TechSupport

the default dts file supports lvds already, which is imx8qm-mek.dtb

 

0 件の賞賛
返信

2,045件の閲覧回数
mallibeerala
Contributor III

Hi,

I am getting following warning "it6263 7-004c: Probe failed. Remote port '/ldb@572410e0/lvds-channel@0' disabled" and at the same time I am getting HDMI display output properly.

Thanks & Regards,
Mallikarjuna B.

0 件の賞賛
返信

2,033件の閲覧回数
joanxie
NXP TechSupport
NXP TechSupport

did you use nxp demo images? imx8qm-mek.dts doesn't enable the hdmi, pls double check if you use the correct dtb file

"https://source.codeaurora.org/external/imx/linux-imx/tree/arch/arm64/boot/dts/freescale/imx8qm-mek.d..."

0 件の賞賛
返信