Hi,
Has anyone tried to build under Ubuntu 11.04? I did "./ltib -c" and immediately got this error
Package Minimum ver Installed info
------------- ------------------ -------------------
zlib 0 not installed
I've installed pretty much all zip related packages in "Ubuntu Softwae Center" and still no luck. Anyone know which package (and how to install) I need?
Thanks
It needs the fixed Ltibutils.pm file as well.
There is no need. I think so!!!
It's not required, in my case.
Regards, J.P.Raja
Would you be interested in give Yocto a try?
https://github.com/Freescale/fsl-community-bsp-platform/blob/master/README
Denzil branch has support for imx53QSB on 11.09
zlib1g as well as zlib1g-dev are already installed. I found help from this thread
However, I think I might messed up my install cause I hit -Ctrl-C when it looked like ltib was hung.
Any one know how to completely re-install ltib from scratch?
Also, I think you should be using the L2.6.35_11.04.01 package. You should be able to port this to the imx53 with little trouble. I did this for the iMX233.
I'm working with the L2.6.35_11.01.01 for the iMx53 Quick Start Board.