LTIB for iMX25 installation error - need help

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LTIB for iMX25 installation error - need help

Jump to solution
2,624 Views
arumugamramasam
Contributor II

Hi,

I am using Ubuntu 9.04 and when i un-tar the LTIB source files and try to run the install script, i am facing error message as attached. Need help to successfully install the LTIB for iMX25. Error messages showing a few packages missing.

LTIBError.png  

Thanks,
Arumugam R

Labels (1)
0 Kudos
Reply
1 Solution
2,313 Views
saurabh206
Senior Contributor III

Hi,

LTIB requires some package to be installed on your UBUNTU machine.

You can use sudo apt-get install m4 bison patch tcl rpm rpm-build.

You can check follow link for LTIB installation.

https://community.freescale.com/docs/DOC-1442

Thanks,

Saurabh

PicusTech Software

View solution in original post

0 Kudos
Reply
2 Replies
2,314 Views
saurabh206
Senior Contributor III

Hi,

LTIB requires some package to be installed on your UBUNTU machine.

You can use sudo apt-get install m4 bison patch tcl rpm rpm-build.

You can check follow link for LTIB installation.

https://community.freescale.com/docs/DOC-1442

Thanks,

Saurabh

PicusTech Software

0 Kudos
Reply
2,313 Views
arumugamramasam
Contributor II

Hi Saurabh,

Thanks for the information… I am able to install the necessary packages and now LTIB configuration is going on. Thanks once again…

Thanks,

Arumugam R

0 Kudos
Reply