LTIB build fails on lkc, using Ubuntu 11.10 and LTIB 9.1.1

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

LTIB build fails on lkc, using Ubuntu 11.10 and LTIB 9.1.1

32,343 次查看
AdCmo
Contributor III

All,

I ran:

./ltib -m config

All the following build OK:

Processing: rpm-fs
Processing: fake-provide
Processing: mkspooflinks
Processing: distcc     
Processing: ccache     
Processing: bison      
Processing: flex       
Processing: texinfo    
Processing: autoconf   
Processing: libtool    
...

LTIB breaks at lkc with this error:

...

Processing: lkc
=================

....

util.c:(.text+0xa58): undefined reference to `winch'
util.c:(.text+0xa6c): undefined reference to `waddch'
util.c:(.text+0xa8b): undefined reference to `wnoutrefresh'
collect2: ld returned 1 exit status
make: *** [mconf] Error 1
error: Bad exit status from /opt/freescale/ltib/tmp/rpm-tmp.33058 (%build)


RPM build errors:
    Bad exit status from /opt/freescale/ltib/tmp/rpm-tmp.33058 (%build)
Build time for lkc: 2 seconds

Failed building lkc
Died at ./ltib line 1380.
traceback:
 main::build_host_rpms:1380
  main::host_checks:1435
   main:542

 

I read somwere that it might be becuase of ncurses.

I installed libncurses5-dev

All,

I ran:

./ltib -m config

All the following build OK:

Processing: rpm-fs
Processing: fake-provide
Processing: mkspooflinks
Processing: distcc     
Processing: ccache     
Processing: bison      
Processing: flex       
Processing: texinfo    
Processing: autoconf   
Processing: libtool    
...

LTIB breaks at lkc with this error:

...

Processing: lkc
=================

....

util.c:(.text+0xa58): undefined reference to `winch'
util.c:(.text+0xa6c): undefined reference to `waddch'
util.c:(.text+0xa8b): undefined reference to `wnoutrefresh'
collect2: ld returned 1 exit status
make: *** [mconf] Error 1
error: Bad exit status from /opt/freescale/ltib/tmp/rpm-tmp.33058 (%build)


RPM build errors:
    Bad exit status from /opt/freescale/ltib/tmp/rpm-tmp.33058 (%build)
Build time for lkc: 2 seconds

Failed building lkc
Died at ./ltib line 1380.
traceback:
 main::build_host_rpms:1380
  main::host_checks:1435
   main:542

----------------------------------------------------

I read somwere that it might be becuase of ncurses.

I installed "libncursesw5-dev" which was picked instead of "libncurses-dev"
and "ncurses-dev" which I tried.

 

Any clues what I am missing?

"/opt/freescale/ltib/tmp/rpm-tmp.33058" is attached:

Thanks,

Ad.

------------------------------

Original Attachment has been moved to: 518-optfreescaleltibtmprpmtmp.33058

标记 (1)
19 回复数

26,523 次查看
kodhel
Contributor II

I have the same problem as well.

I am running on ubuntu 16.04 and I have applied the patches suggested above.

I still see the same issue listed below:

gcc conf.o zconf.tab.o -o conf
143 zconf.tab.o: In function `menu_re_search':
144 /opt/freescale/ltib/usr/src/rpm/BUILD/lkc-1.4/menu.c:416: undefined reference to `next_id'
145 /opt/freescale/ltib/usr/src/rpm/BUILD/lkc-1.4/menu.c:427: undefined reference to `next_id'
146 collect2: error: ld returned 1 exit status
147 Makefile:106: recipe for target 'conf' failed
148 make: *** [conf] Error 1
1

0 项奖励
回复

26,523 次查看
meandyoursame
Contributor I

How do use patch file?

0 项奖励
回复

26,515 次查看
Yuri
NXP Employee
NXP Employee

Hello,

  Please follow enclosed "Setting_up_a_Linux_Host_for_LTIB_Builds_on_Ubuntu_9.04.pdf".

Regards,

Yuri.

0 项奖励
回复

26,515 次查看
bba
Contributor III

Hi Curtis,

Thank you very much, with your patches according to the lkc, sparse and mux_server packages LTIB is running on xubuntu-12.04-64Bit.

@Ad 

I'm using elftosb-version 10.12.02, so no modifications were necessary on these package.

Regards

0 项奖励
回复

26,515 次查看
glenfine
Contributor I

I'd like to thank the person who came up with the oneiric-ltib-patch. Works great. 

But then I use Ubuntu 12.04 LTS on VMWARE, and I end up an error complaining about  .gvfs and premission denied.  Anyone have a workaround? or patch?

I have tried 'chmod 777 /home/user/.gvfs' and './ltib --continue' but can not get past this point.

Evidently fuse has the resource mounted and I will always get a 'permission denied'. 

Here is the error I get.

[fluff removed]..

+ umask 022

+ cd /opt/freescale/ltib/usr/src/rpm/BUILD

+ cd mux_sever-1.0

+ rm -rf /home/user/ltib/ltib-mpc5121ads-20090602/tmp/mux_sever

+ exit 0

Executing(--clean): /bin/sh -e /home/user/ltib/ltib-mpc5121ads-20090602/tmp/rpm-tmp.65905

+ umask 022

+ cd /opt/freescale/ltib/usr/src/rpm/BUILD

+ rm -rf mux_sever-1.0

+ exit 0


Build time for mux_server: 2 seconds

sudo /opt/freescale/ltib/usr/bin/rpm --root / --dbpath /opt/freescale/ltib/var/lib/rpm -e --allmatches --nodeps --define '_tmppath /home/user/ltib/ltib-mpc5121ads-20090602/tmp' mux_sever 2>/dev/null

sudo /opt/freescale/ltib/usr/bin/rpm --root / --dbpath /opt/freescale/ltib/var/lib/rpm --prefix / --ignorearch -ivh --replacepkgs --replacefiles --nodeps --excludedocs --define '_tmppath /home/user/ltib/ltib-mpc5121ads-20090602/tmp' /opt/freescale/ltib/usr/src/rpm/RPMS/x86_64/mux_sever-1.0-1.x86_64.rpm

error: failed to stat /home/user/.gvfs: Permission denied

Preparing...                ##################################################

mux_sever                   ##################################################


0 项奖励
回复

26,515 次查看
Gavroche
Contributor I

Further to Curtis's post I found I needed to do the following, after installing his patch,  to clear out the old failed build.

sudo rm -rf /opt/freescale/ltib/usr/src/rpm/BUILD/*

 

(I'm using Ubuntu 12.04)

0 项奖励
回复

26,515 次查看
caohaifeng
Contributor IV

Hi Duncan,

I have tried the Curtils' path,and sudo rm -rf /opt/freescale/ltib/usr/src/rpm/BUILD/*

but the error is still exist,the content of host_config.log is the same as Adolph's。

I'm using Ubuntu 12.04 too.

How to solve it?

Thank you

0 项奖励
回复

26,515 次查看
VJ96
Contributor II
0 项奖励
回复

26,515 次查看
MattEdinger
Contributor I

"Precise Pangolin" is the code name for Ubuntu 12.04, scheduled for release on 26 April 2012.

 

https://wiki.ubuntu.com/PrecisePangolin


Krishna Pavan said:

Hi Ad,

 

If your idea to downgrade to 10.04 is due to the reason that 10.04 is LTS, then you can try 12.04 [Precise Pangolin] which is also a LTS.

 

Regards    Krishna Pavan

0 项奖励
回复

26,515 次查看
KrishnaPavan
Contributor II

Hi Ad,

 

If your idea to downgrade to 10.04 is due to the reason that 10.04 is LTS, then you can try 12.04 [Precise Pangolin] which is also a LTS.

 

Regards    Krishna Pavan

0 项奖励
回复

26,515 次查看
AdCmo
Contributor III

Curtis,

Thanks, your solution went a long way in the build.

My build now fails down the line when trying to build elftosb.


I found what the problem is with that.
But that fundamental error makes me lose trust in the source code.
They seem to have hard coded paths in the C code itself !!!


Processing: elftosb
=====================
Build path taken because: no prebuilt rpm,

...
etc.
...

-rw-rw-r-- root/root        33 2011-02-28 21:05 elftosb-11.09.01/test_files/test0.key
drwxrwxr-x root/root         0 2011-02-28 21:05 elftosb-11.09.01/winsupport/
-rw-rw-r-- root/root         0 2011-02-28 21:05 elftosb-11.09.01/winsupport/unistd.h
+ STATUS=0
+ [ 0 -ne 0 ]
+ cd elftosb-11.09.01
+ exit 0
Executing(%build): /bin/sh -e /opt/freescale/ltib/tmp/rpm-tmp.4660
+ umask 022
+ cd /opt/freescale/ltib/usr/src/rpm/BUILD
+ cd elftosb-11.09.01
+ make
make -C bld/linux -f /opt/freescale/ltib/usr/src/rpm/BUILD/elftosb-11.09.01/makefile.rules SRC_DIR=/opt/freescale/ltib/usr/src/rpm/BUILD/elftosb-11.09.01 all;
make[1]: Entering directory `/opt/freescale/ltib/usr/src/rpm/BUILD/elftosb-11.09.01/bld/linux'
gcc -g -I/opt/freescale/ltib/usr/src/rpm/BUILD/elftosb-11.09.01/elftosb2 -I/opt/freescale/ltib/usr/src/rpm/BUILD/elftosb-11.09.01/keygen -I/opt/freescale/ltib/usr/src/rpm/BUILD/elftosb-11.09.01/sbtool -I/opt/freescale/ltib/usr/src/rpm/BUILD/elftosb-11.09.01/common -DLinux -c /opt/freescale/ltib/usr/src/rpm/BUILD/elftosb-11.09.01/common/AESKey.cpp
In file included from /opt/freescale/ltib/usr/src/rpm/BUILD/elftosb-11.09.01/common/AESKey.h:10:0,
                 from /opt/freescale/ltib/usr/src/rpm/BUILD/elftosb-11.09.01/common/AESKey.cpp:8:
/opt/freescale/ltib/usr/src/rpm/BUILD/elftosb-11.09.01/common/stdafx.h:30:36: fatal error: /usr/include/sys/types.h: No such file or directory
compilation terminated.
make[1]: *** [AESKey.o] Error 1
make[1]: Leaving directory `/opt/freescale/ltib/usr/src/rpm/BUILD/elftosb-11.09.01/bld/linux'
make: *** [all] Error 2
error: Bad exit status from /opt/freescale/ltib/tmp/rpm-tmp.4660 (%build)

RPM build errors:
    Bad exit status from /opt/freescale/ltib/tmp/rpm-tmp.4660 (%build)
Build time for elftosb: 1 seconds

Failed building elftosb
Died at ./ltib line 1380.
traceback:
 main::build_host_rpms:1380
  main::host_checks:1435
   main:542

Obviously the path in 11.10 has changed from:

"/usr/include/sys/types.h"
to
"/usr/include/i386-linux-gnu/sys/types.h"

Who still hard codes "#includes" using a complete path?

Anyway ... I will fix this release on my time later,

For now I am downgrading to 10.04.

Ad.
-------------------------

0 项奖励
回复

26,515 次查看
KrishnaPavan
Contributor II

Hi Daiane,

 

I doubt, these installations all go well only with LTS Versions from Ubuntu.

 

Is it the way, because 10.04 LTS, 12.04 LTS etc., have no problems it seems.... Is it problem with the versions?

0 项奖励
回复

26,515 次查看
daiane_angolini
NXP Employee
NXP Employee

I'm using Ubuntu 10.10 (Maverick Meerkat)  for LTIB and Android build and it works

0 项奖励
回复

26,515 次查看
hake
NXP Employee
NXP Employee

ubuntu 9.10 offically. but I once test with 10.10 which works too.

0 项奖励
回复

26,515 次查看
CurtisWald
NXP Employee
NXP Employee

I was able to execute ltib on Ubuntu 11.10 creating a minimum file system.  I was working with an i.mx35 release L2.6.31_09.12.01_SDK_source.tar.gz but solution should work with an i.mx5x or i.mx6x.

The issue with lkc was the ordering in the link command for the curses library.
Here is a summary and patches I used to build:


Description    : Install patches correcting ltib execution on Ubuntu 11.10.
Host        : Oneiric Ubuntu 11.10 64-bit
LTIB version    : ./ltib --version
ltib 9.1.1 ($Revision: 1.445.6.1 $)
Copyright (C) 2004-2006 Freescale Semiconductor, Inc.
This is free software; it is licensed under the terms of the
GNU General Public License, see 'COPYING' for the license.  There is NO
warranty; not even for MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE.


When ltib fails when trying to build the lkc package:

1) Extract the contents of oneiric-ltib-patch.tgz at the same directory
   level as ltib.

    $ tar -zxf oneiric-ltib-patch.tgz
    $ ls -1
    oneiric-ltib-patch
    ltib

2) Run the script install-patches.sh found in oneiric-ltib-patch:

       $ cd oneiric-ltib-patch
       $ ./install-patches.sh

Read the file install-patches.sh and you will see additional comments and
the exact changes that were made. Additional packages were patched and
modified, you just have not gotten to that part yet :)

4) After installing the patches, run ./ltib and this was able to build all.

26,515 次查看
Albert1z
Contributor II

Can Ubuntu 11.04 work with LTIB? I need to know as well so that I can install the right version. Otherwise, a lot of time will be wasted.

0 项奖励
回复

26,515 次查看
AdCmo
Contributor III

Hake,

Can you please list the latest versions of Ubuntu and/or Fedora
that are guaranteed/known to work with LTIB 9.1.1 on i.MX53 at least?

Thanks,

Ad.

----------------------------

 

hake huang said:

LTIB doed not support 11.10 build host, that's the current status

0 项奖励
回复

26,515 次查看
AdCmo
Contributor III

Hake,

I am aware of that.

Do you have a list of the latest versions of Ubuntu and Fedora that are supported?

These are generic problems and I intend to make it work :)

I have already gone far enough.

 

Ad.

--------------------

0 项奖励
回复

26,515 次查看
hake
NXP Employee
NXP Employee

LTIB doed not support 11.10 build host, that's the current status

0 项奖励
回复