Hi,
I am getting below error when building gtk+(2.20.1). I have built successfully all X11 packages and Cairo(1.6.4), Pango( 1.20.5), Atk(1.29.2). Please guide.
Regards,
Swamy
checking for BASE_DEPENDENCIES... yes
checking for CAIRO_BACKEND... configure: error: Package requirements (cairo-xlib >= 1.6) were not met:
No package 'cairo-xlib' found
Consider adjusting the PKG_CONFIG_PATH environment variable if you
installed software in a non-standard prefix.
Alternatively, you may set the environment variables CAIRO_BACKEND_CFLAGS
and CAIRO_BACKEND_LIBS to avoid the need to call pkg-config.
See the pkg-config man page for more details.
error: Bad exit status from /mnt/freescale/ltib_git/ltib/tmp/rpm-tmp.15404 (%build)
RPM build errors:
Bad exit status from /mnt/freescale/ltib_git/ltib/tmp/rpm-tmp.15404 (%build)
Build time for gtk2: 7 seconds
Failed building gtk2
f_scbuild() returned an error, exiting
traceback:
main:611
解決済! 解決策の投稿を見る。
Did you have any luck?
Thanks for the reply. I was able to fix this issue. As some of the packages including libcairo2-dev was missing.. Thanks
Could you please select the Correct Answer and mark your question as Answered if it is. Thanks!
Have you installed libcairo2-dev