LTIB build Error

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

LTIB build Error

856 次查看
vijayk
Contributor I

I am trying to build the LTIB. I am getting the following error

cd /opt/freescale/ltib/usr/src/rpm/BUILD

cd: 1: can't cd to /opt/freescale/ltib/usr/src/rpm/BUILD

error: Bad exit status from /home/vijay/work/IMX_6/source_code/L3.0.35_12.09.01_GA_source/ltib/tmp/rpm-tmp.16642 (%prep)

RPM build errors:

    Bad exit status from /home/vijay/work/IMX_6/source_code/L3.0.35_12.09.01_GA_source/ltib/tmp/rpm-tmp.16642 (%prep)

Build time for fake-provides: 0 seconds

Failed building fake-provides

Died at ./ltib line 1392.

traceback:

main::build_host_rpms:1392

  main::host_checks:1447

   main:554


标签 (1)
0 项奖励
回复
0 回复数