Hello,
I have a iMX6 Sabrelite development board. I have a Ltib 2,6,38 version for the same board.
While compiling on 64 bit Ubuntu 12,04LTS , I find the build fails because of gtk error (f_buildrpms() returned an error,) been repeated ...
Further I have checked in internet and tried some solutions like installing all packages related to gtk, cairo etc and other solutions like bash, building cairo before ./ltib, but I fail to build the LTIB with the same error....
In the ./ltib -m config , I even cannot disable gtk and cairo.
Can you please suggest and idea or solution?
Please give some solutions, I am stuck since a long time.
The following is a brief report of the failed build.
checking for libpng12... yes
checking pixbuf loaders to build...
checking immodules to build...
checking for sys/wait.h that is POSIX.1 compatible... yes
checking return type of signal handlers... (cached) void
checking sys/systeminfo.h usability... no
checking sys/systeminfo.h presence... no
checking for sys/systeminfo.h... no
checking sys/sysinfo.h usability... yes
checking sys/sysinfo.h presence... yes
checking for sys/sysinfo.h... yes
checking for mediaLib 2.3... checking for mlib_ImageSetStruct in -lmlib... no
checking for x86 platform... no
checking for gdk-pixbuf-csource... /usr/bin/gdk-pixbuf-csource
checking for gtk-update-icon-cache... /usr/bin/gtk-update-icon-cache
checking for X... no
configure: error: X development libraries not found
error: Bad exit status from /home/praveen/freescale/ltib/tmp/rpm-tmp.26100 (%build)
RPM build errors:
Bad exit status from /home/praveen/freescale/ltib/tmp/rpm-tmp.26100 (%build)
Build time for gtk2: 15 seconds
Failed building gtk2
f_buildrpms() returned an error, exiting
traceback:
main:560
Started: Mon Oct 22 00:08:17 2012
Ended: Mon Oct 22 00:08:33 2012
Elapsed: 16 seconds
These packages failed to build:
gtk2
Build Failed