LTIB Build Error

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

LTIB Build Error

1,700 次查看
arunachalamrama
Contributor III

I am able to build L3.0.35_4.1.0 on Ubuntu 14.04.

After applying Multimedia Codec, I get error given below.

I tried different solutions suggested in freescale community and other websites. Problem is still there.

Please let me know if this can be solved or another Linux version with Multimedia Codec (gstreamer) support.

Regards,

Arun

Processing: fsl-alsa-plugins

==============================

Build path taken because: no prebuilt rpm,

Testing network connectivity

OK GPP:

Try fsl-alsa-plugins-1.0.25.tar.gz.md5 from the GPP

http://bitshrine.org/gpp/fsl-alsa-plugins-1.0.25.tar.gz.md5:

02:03:28 ERROR 404: Not Found.

Try fsl-alsa-plugins-1.0.25.tar.gz from the GPP

http://bitshrine.org/gpp/fsl-alsa-plugins-1.0.25.tar.gz:

02:03:28 ERROR 404: Not Found.

Can't get: fsl-alsa-plugins-1.0.25.tar.gz at ./ltib line 802.

f_buildrpms() returned an error, exiting

traceback:

main:572

Started: Thu Apr 21 02:00:05 2016

Ended:   Thu Apr 21 02:03:28 2016

Elapsed: 203 seconds

These packages failed to build:

fsl-alsa-plugins

Build Failed

Exiting on error or interrupt

标签 (3)
0 项奖励
回复
3 回复数

1,444 次查看
jimmychan
NXP TechSupport
NXP TechSupport

I would suggest you to use Yocto BSP. LTIB is old and will not have any new BSP release.

0 项奖励
回复

1,444 次查看
arunachalamrama
Contributor III

Thanks, jimmychan, for the  update and suggestion.

Please suggest Yocto version with gstreamer support.

Arun

0 项奖励
回复

1,444 次查看
arunachalamrama
Contributor III

Downloaded Linux source and MM Codec source from this link: i.MX 6 Q/D/DL/S L3.0.35_4.1.0 GA release

0 项奖励
回复