I am able to build L3.0.35_4.1.0 on Ubuntu 14.04.
After applying Multimedia Codec, I get error given below.
I tried different solutions suggested in freescale community and other websites. Problem is still there.
Please let me know if this can be solved or another Linux version with Multimedia Codec (gstreamer) support.
Regards,
Arun
Processing: fsl-alsa-plugins
==============================
Build path taken because: no prebuilt rpm,
Testing network connectivity
OK GPP:
Try fsl-alsa-plugins-1.0.25.tar.gz.md5 from the GPP
http://bitshrine.org/gpp/fsl-alsa-plugins-1.0.25.tar.gz.md5:
02:03:28 ERROR 404: Not Found.
Try fsl-alsa-plugins-1.0.25.tar.gz from the GPP
http://bitshrine.org/gpp/fsl-alsa-plugins-1.0.25.tar.gz:
02:03:28 ERROR 404: Not Found.
Can't get: fsl-alsa-plugins-1.0.25.tar.gz at ./ltib line 802.
f_buildrpms() returned an error, exiting
traceback:
main:572
Started: Thu Apr 21 02:00:05 2016
Ended: Thu Apr 21 02:03:28 2016
Elapsed: 203 seconds
These packages failed to build:
fsl-alsa-plugins
Build Failed
Exiting on error or interrupt
Thanks, jimmychan, for the update and suggestion.
Please suggest Yocto version with gstreamer support.
Arun
Downloaded Linux source and MM Codec source from this link: i.MX 6 Q/D/DL/S L3.0.35_4.1.0 GA release