LPDDR5 application with i.MX 9 series

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

LPDDR5 application with i.MX 9 series

跳至解决方案
1,396 次查看
Maxjay
Contributor II

Hi NXP,

How many LPDDR5 chips can be connect with i.MX 94 or i.MX 95? 

Thank you.

0 项奖励
回复
1 解答
1,369 次查看
AldoG
NXP TechSupport
NXP TechSupport

Hello,

Please note that both chips are still under pre-prodcution stage so any specifications and information herein are subject to change without notice. For additional information contact your sales representative.

For the i.MX94
Up to 4.2GT/s x32 LPDDR4/LPDDR5 (with Inline ECC) are supported.

For the i.MX95
Up to 6.4GT/s x32 LPDDR5/LPDDR4X (with Inline ECC & Inline Encryption)

Best regards/Saludos,
Aldo.

在原帖中查看解决方案

0 项奖励
回复
2 回复数
1,308 次查看
Maxjay
Contributor II

Thanks for your information!

1,370 次查看
AldoG
NXP TechSupport
NXP TechSupport

Hello,

Please note that both chips are still under pre-prodcution stage so any specifications and information herein are subject to change without notice. For additional information contact your sales representative.

For the i.MX94
Up to 4.2GT/s x32 LPDDR4/LPDDR5 (with Inline ECC) are supported.

For the i.MX95
Up to 6.4GT/s x32 LPDDR5/LPDDR4X (with Inline ECC & Inline Encryption)

Best regards/Saludos,
Aldo.

0 项奖励
回复