LPDDR5 application with i.MX 9 series

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPDDR5 application with i.MX 9 series

ソリューションへジャンプ
1,353件の閲覧回数
Maxjay
Contributor II

Hi NXP,

How many LPDDR5 chips can be connect with i.MX 94 or i.MX 95? 

Thank you.

0 件の賞賛
返信
1 解決策
1,326件の閲覧回数
AldoG
NXP TechSupport
NXP TechSupport

Hello,

Please note that both chips are still under pre-prodcution stage so any specifications and information herein are subject to change without notice. For additional information contact your sales representative.

For the i.MX94
Up to 4.2GT/s x32 LPDDR4/LPDDR5 (with Inline ECC) are supported.

For the i.MX95
Up to 6.4GT/s x32 LPDDR5/LPDDR4X (with Inline ECC & Inline Encryption)

Best regards/Saludos,
Aldo.

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,265件の閲覧回数
Maxjay
Contributor II

Thanks for your information!

1,327件の閲覧回数
AldoG
NXP TechSupport
NXP TechSupport

Hello,

Please note that both chips are still under pre-prodcution stage so any specifications and information herein are subject to change without notice. For additional information contact your sales representative.

For the i.MX94
Up to 4.2GT/s x32 LPDDR4/LPDDR5 (with Inline ECC) are supported.

For the i.MX95
Up to 6.4GT/s x32 LPDDR5/LPDDR4X (with Inline ECC & Inline Encryption)

Best regards/Saludos,
Aldo.

0 件の賞賛
返信