LPDDR4

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

LPDDR4

1,124 次查看
EErdem
Contributor I

Hello,

 

We are designing a single board computer using i.MXX8MM Soc.

In our case, we have 2 GB LPDDR4 which is the same as the EVK.

My Stack Up is

Top Layer Signal ( some of DDR data signals)

Mid Layer 1 GND

Mid Layer 2 SİGNAL ( Some of DDR data signals)

Mid Layer 3 POWER(DDR Main Power)

Mid layer 4  GND

Mid Layer 5 Signal(DDR Clock)

Mid layer 6 1.8V Power

Bottom Layer Signal

 

From the hardware design guide, what I understand mid layer 2 and mid-layer 5 should have a solid ground plane both above and below.

Q1: Must I provide a ground plane for both mid layer 3 and mid layer 6.

Q2: Is it enough to provide a ground plane just only one side rather than both sides.

Q3: Could you answer the second question for MIPI, USB, PCIe, SDIO, etc.

Q4 : Also , we want to use 4GB LPDDR4 that have same package with EVK LPDDR4(MT53D512M32D2DS-053 AUT: D) Do you suggest any of LPDDR4 (From the NXP community we found that MT53D1024M32D4DT-053 can be fit could you check it?)

 

Note : To be more clear I have attached a word file which shows the layer order and routing for LPDDR4 layout.)

0 项奖励
回复
1 回复

1,120 次查看
igorpadykov
NXP Employee
NXP Employee

Hi EErdem

 

1. no

2. for 2 ,5 layers it is necessary on both sides.

3. please follow recommendations given in i.MX 8M Mini Hardware Developer’s Guide

4. yes MT53D1024M32D4DT-053 can be used.

 

Best regards
igor

0 项奖励
回复