LPDDR4 capacity for MIMX8QM6AVUFFAB

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPDDR4 capacity for MIMX8QM6AVUFFAB

1,497件の閲覧回数
tw_wang
Contributor I

Could we change the  LPDDR4 capacity from 6GB to the 4GB or 8GB on the MIMX8QM6AVUFFAB referece design ?

0 件の賞賛
返信
4 返答(返信)

1,468件の閲覧回数
Mestkim
Contributor III

i.MX 8/8X Family DDR Tools Release - NXP Community

 

3. Change 0x980000000 to 0xA00000000 in the above chunk of code. That should allow for 8GB density for MX8QM example shown above (for MX8QXP, change 0x8C0000000ULL to 0x900000000ULL for 4GB density).

0 件の賞賛
返信

1,480件の閲覧回数
joanxie
NXP TechSupport
NXP TechSupport
0 件の賞賛
返信

1,466件の閲覧回数
Mestkim
Contributor III

i.MX8QM MEK board is 6GB. 

tw wang knows the i.MX8QM MEK is 6GB.

But you don't know.

and you don't know what is per controller in i.MX 8/8X/8XLite - LPDDR4 and DDR3L memory compat... - NXP Community 

 

0 件の賞賛
返信

1,445件の閲覧回数
joanxie
NXP TechSupport
NXP TechSupport

yes, the imx8qm supports 4GB(per controller) max, this is my misunderstanding, I thought tw_wang needs 8GB/controller, for total 8GB, this is patch

SCFW lilmits the DDR size to 6GB both in DDR tool and Linux BSP.

1. Replace mx8qmb0_scfw_download.bin in DDR_tool/bin with the attached binary. You can stress test all 8GB memory size with your DDR script.

2. Modify board_system_config() in board.c in your SCFW project as follows

/* Board has 6GB8GB memory so fragment upper region and retain 4GB */

        BRD_ERR(rm_memreg_frag(pt_boot, &mr_temp, 0x980000000ULL, 0xA00000000ULL,

            0xFFFFFFFFFULL));

0 件の賞賛
返信