customer is LGE-CTO
project is IFE (In Flight Entertainment)
silicon : i.MX8MQ
BSP : L5.4.70.
issue : customer met booting failure with suck at "starting kernel ...." log.
customer applied below patch and with ddr_timing.c from ddr stress tool.
with below patch + removed OPTEE ==> 4G booting is okay and also 4G memory seems to be okay on target board.
But, below patch + OPTEE , customer met booting failure with stuck at "starting kernel.."
diff -urN a/arch/arm/dts/imx8mq-evk.dts b/arch/arm/dts/imx8mq-evk.dts memory@40000000 { pcie0_refclk: pcie0-refclk { |
diff -urN a/configs/imx8mq_evk_defconfig b/configs/imx8mq_evk_defconfig #define CONFIG_SYS_SDRAM_BASE 0x40000000
below is bdinfo with booting failure. i am not sure but does below glue text address is as below. it is for your reference. u-boot=> bdinfo
Could you please check this issue and help me to find any clue? Thank you BRs jessie |
解決済! 解決策の投稿を見る。
We had a way to support 8MQ 4GB memory without changing OPTEE load address.
Please refer to: https://community.nxp.com/t5/iMX-and-Vybrid-Support/8M-Scale-845-850-board-4GB-memory-support-summar...
Hi @kevin_fu :
I don't know what's your exact request, any way I past below for your reference:
ifneq (,$(filter $(PLATFORM_FLAVOR),mx8mqevk))
-CFG_DDR_SIZE ?= 0xc0000000
+CFG_DDR_SIZE ?= 0x100000000
+CFG_TZDRAM_START ?= 0xfe000000
CFG_UART_BASE ?= UART1_BASE
+$(call force,CFG_CORE_LARGE_PHYS_ADDR,y)
+$(call force,CFG_CORE_ARM64_PA_BITS,36)
endif
We had a way to support 8MQ 4GB memory without changing OPTEE load address.
Please refer to: https://community.nxp.com/t5/iMX-and-Vybrid-Support/8M-Scale-845-850-board-4GB-memory-support-summar...
Can you share the link? No access。
You do not have sufficient privileges for this resource or its parent to perform this action. Click your browser's Back button to continue.
Can you share the link? No access。