[LGE-/Aircon/i.MX6DQ_SDB] optimized kernel configuration

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

[LGE-/Aircon/i.MX6DQ_SDB] optimized kernel configuration

Jump to solution
860 Views
Jessie_Lee
NXP Employee
NXP Employee

Hi team

our customer is LGE-HA (Home Appliance)

BSP : L4.14.98

CPU: i.mx6dq_sabresd

customer enable display feature with adding some kernel configuration

They do not backend server. LGE use FB with QT app.

They observed memory increased after adding FB related configuration. increased memory size is about 60MB without any QT application run. 

It seems... only kernel configuration cause 60MB memory increasion

This display added project is based on previous NO display project.

So, i attached two configuration files, one is no display and another is enablement FB related.

rrc_defconfig_20201005_FB_Enablement.txt : for display feature

cgw_defconfig_20101005.txt : No Display project.

Could you please check these defconfig file and guide unnecessary configuration which could be removed from default FB operation. 

 

 

 

 

0 Kudos
1 Solution
856 Views
Jessie_Lee
NXP Employee
NXP Employee

I should close this ticket. moved other space.

 

BRs

jessie

View solution in original post

0 Kudos
1 Reply
857 Views
Jessie_Lee
NXP Employee
NXP Employee

I should close this ticket. moved other space.

 

BRs

jessie

0 Kudos