Can someone please give me some direction on controlling the LEDs (and maybe other GPIOs) on the iMX8QM-MEK board from both U-Boot (in code) and Linux (maybe from the command line)?
I'm having a hard time finding it in the docs.
Thank you
Igor, thank you. I will look into this.
Igor, thank you again for this.
Unfortunately, I am having trouble doing something which I think is quite basic. Here are the specifics. Perhaps you can show me the proper steps or an example?
In U-boot, I would like to control the SCU Debug LED (which is D3 on the iMX8QM-MEK schematic). This LED is tied to SCU_GPIO0_02.
From what I've figured out from the U-Boot source, I think I need to do some combination of changing the DTS, "allocating" a resource, reserving a resource, and setting a pad configuration, but I just can't figure it out.
Thank you very much!
Stuart
Hi Stuart
may be useful to look:
System Controller Firmware 101 - Pad configuration service
dts example
fsl-imx8q-arm2.dtsi\freescale\dts\boot\arm64\arch - linux-imx - i.MX Linux kernel
pinctrl_pcieb: pciebgrp{
fsl,pins = <
SC_P_PCIE_CTRL1_CLKREQ_B_LSIO_GPIO4_IO30 0x06000021
SC_P_PCIE_CTRL1_WAKE_B_LSIO_GPIO4_IO31 0x04000021
SC_P_PCIE_CTRL1_PERST_B_LSIO_GPIO5_IO00 0x06000021
>;
};
&pcieb{
ext_osc = <1>;
pinctrl-names = "default";
pinctrl-0 = <&pinctrl_pcieb>;
reset-gpio = <&gpio5 0 GPIO_ACTIVE_LOW>;
clkreq-gpio = <&gpio4 1 GPIO_ACTIVE_LOW>;
status = "okay";
};
Best regards
igor
Best regards
igor
Hi Stuart
in i.MX8QM (and i.MX8QXP) gpios are handles by SCU: System Controller Firmware 101 - Getting started
documentation can be found in SCFW Porting Kit
May be useful similar case https://community.nxp.com/thread/511052
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------