LCDIF and Host Display controller support in U-boot for i.MX8M Mini

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LCDIF and Host Display controller support in U-boot for i.MX8M Mini

1,107 Views
kailas_kharse
Contributor IV

Hello,

I am in process of porting the LCD with the MIPI interface in U-boot, Display works properly in Kernel.

I want to understand that do we have the support of LCDIF and Host display controller in U-boot?

How can I port the MIPI-Display in U-boot? Do you have any working reference to port MIPI-Display in U-boot?


Thanks & Regards,
Kailas K

Tags (1)
0 Kudos
Reply
2 Replies

1,101 Views
igorpadykov
NXP Employee
NXP Employee

Hi Kailas

 

one can look at below example (for RM67191), for custom lcd timings can be added to

struct display_info_t const displays[]

https://source.codeaurora.org/external/imx/uboot-imx/tree/board/freescale/imx8mm_evk/imx8mm_evk.c?h=...

#ifdef CONFIG_VIDEO in

https://source.codeaurora.org/external/imx/uboot-imx/tree/include/configs/imx8mm_evk.h?h=imx_v2019.0...

 

Best regards
igor

0 Kudos
Reply

1,084 Views
kailas_kharse
Contributor IV
Hello Igor,

We already have tried adding the structure and enabled the CONFIG_VIDEO in defconfig and also instead of adding

CONFIG_VIDEO_MXS=y
CONFIG_RM67191=y

no rm67191.o is getting generated. I think we are missing something can you share all the configs and dts for imx8mm and anything else that will be required to get the panel up.


Thanks & Regards
Kailas Kharse
 
 
0 Kudos
Reply