Hi all-
I have some strange behavior on my board and LCD
It's a custom iMX6S board running Linux 3.0.35. The display is a parallel LCD (8-bit) using BT656 protocol.
After booting, I display an image on the LCD. After a few minutes the display suddenly becomes white. At that point, if I try to display a new image nothing happens.
However, if I do "echo 0 > /sys/devices/platform/mxc_sdc_fb.0/graphics/fb0/blank", then I can display images again. But, again, after a few minutes the LCD turns white.
Any ideas what might be causing the LCD to 'turn white' by itself?
Sincerely,
Erez
已解决! 转到解答。
Hi Erez
one can try to turn off LCD blanking also with
echo -e "\033[9;0]" > /dev/tty0
https://community.freescale.com/message/432351#432351
Best regards
igor
Hi Erez
one can try to turn off LCD blanking also with
echo -e "\033[9;0]" > /dev/tty0
https://community.freescale.com/message/432351#432351
Best regards
igor
Hi Igor,
Thanks -- that solved the issue.
I found this resource with additional useful commands --- http://www.armadeus.com/wiki/index.php?title=FrameBuffer
For anyone looking::
# echo 0 > /sys/class/graphics/fbcon/cursor_blink
also possible at boot time (with 3.x recent kernels):
BIOS> setenv extrabootargs vt.global_cursor_default=0
# echo 1 > /sys/class/graphics/fbcon/cursor_blink
# echo 1 > /sys/class/graphics/fb0/blank
# echo 0 > /sys/class/graphics/fb0/blank
# echo -e '\033[9;X]' > /dev/tty1 (from serial console)
or
# echo -e '\033[9;X]' (from framebuffer console)
or to set it at each boot, use /etc/inittab:
tty1::sysinit:echo -e '\033[9;X]'
# echo -e '\033[?17;0;0c' > /dev/tty1 (from serial console)
or
# echo -e '\033[?17;0;0c' (from framebuffer console)
# echo -e '\033[?5h' > /dev/tty1
# echo -e '\033[?5l' > /dev/tty1
Regards,
Erez