LCD and GPU on i.MX6Solox

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LCD and GPU on i.MX6Solox

1,048 Views
Musadjan
Contributor III

Hi NXP, 

I need to understand differences between i.MX6Solox SoCs part no.  MCIMX6X1CVO08AC  and MCIMX6X3CVO08AC in terms of LCD interface. After reading information about LCD interface of the SoC in page 3 on the datasheet of the i.MX6solox , I came to conclusion that I must use SoC configuration  MCIMX6X3CVO08AC  in order to be able to implement a 7 in 24-bit display using LCD parallel interface on that SoC. The evidence for my decision is that the part MCIMX6X1CVO08AC   does not support 2D/3D GPU according to the datasheet. I would be happy if you could help me to confirm that I made right decision. or in the other world , may the part MCIMX6X1CVO08AC includes a LCD interface which can be used with that display for simple graphical tasks, like showing texts and labels.  Looking forward your feedback and thanks. 

Labels (1)
0 Kudos
Reply
1 Reply

1,006 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello Alim,

You are correct the  MCIMX6X3CVO08AC has the GPU 2D.

Regards

0 Kudos
Reply