LCD Screen iMX RT1170 EV Board

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LCD Screen iMX RT1170 EV Board

915 Views
TM_MI
Contributor III

Hello,

Does the schematic for the evaluation board RT1170 includes only the connection for the LCD screen without the touch panel?

Looking at data sheet for the default LCD used shows 6 pins FCP connector for the CTP.

TM_MI_0-1642627124724.pngTM_MI_1-1642627153748.png

 

Thanks,

Tarek

0 Kudos
4 Replies

904 Views
b36401
NXP Employee
NXP Employee
0 Kudos

892 Views
TM_MI
Contributor III

Hi @b36401 

I have checked the Data sheet and the LCD does include a touch panel; however the schematic here does not include the connection for the touch panel but only the 40 pins for the LCD display.

My first assumption was that I2C5_SDA, I2C5_SCLand CTP_INT are the connection for the touch panel, but I think they are used for “Extended Display Identification Data”

Please correct me if I am wrong.

Thanks,

Tarek

0 Kudos

887 Views
jeremyzhou
NXP Employee
NXP Employee

Hi @TM_MI ,
Your instinct is right, the CTP_SDA and CTP_SCL are used to fetch the touch position of LCD.
BR,
Jeremy

0 Kudos

881 Views
TM_MI
Contributor III

Hello @jeremyzhou 

Thank you.

To clarify things, The CTP pins 1-6 shown on the datasheet are used for the touch panel and the FPC pins 26-29 are also used for the touch panel, but the CTP 1-6 pins are connected internally to 26-29.

So, another connection other than the FPC 40 (Pins 26-29) is not needed to connect to the touch panel.

 

TM_MI_0-1642776636332.png

 

Regards,

Tarek

0 Kudos