Hello,
In order to drive a LCD screen connected to an iMX7 I need to drive the Reset (Bit 0) of LCDIFx_CTRL1n register. I would like to know if this pin is automatically managed by the Linux LCD management stack or I need to control it manually.
If Linux driver manages this pin automatically, in which case the LCD would be reset?
Thanks in advance for your help.
Hi Jean-Baptiste
for lcd pins usage one can look at lcdif driver sources, described in
sect.6.3.4.4 Source Code Structure attached Linux manual and
linux sources on
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------