LCD Reset pin management on iMX7

cancel
Showing results for 
Search instead for 
Did you mean: 

LCD Reset pin management on iMX7

321 Views
jbaptiste_marie
Contributor I

Hello,

In order to drive a LCD screen connected to an iMX7 I need to drive the Reset (Bit 0) of LCDIFx_CTRL1n register. I would like to know if this pin is automatically managed by the Linux LCD management stack or I need to control it manually.

If Linux driver manages this pin automatically, in which case the LCD would be reset?

Thanks in advance for your help.

Labels (3)
0 Kudos
1 Reply

255 Views
igorpadykov
NXP TechSupport
NXP TechSupport

Hi Jean-Baptiste

for lcd pins usage one can look at lcdif driver sources, described in

sect.6.3.4.4 Source Code Structure attached Linux manual and

linux sources on

linux-imx - i.MX Linux kernel 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos