Dear All,
I want to perform the LCD 180 degree rotation in i.MX25.
For this, I confirmed the x-axis rotation with the LPCR and LSSAR register setting.
But, I couldn't find the y-axis rotation for LCD 180 degree rotation.
For the register setting, refer to the "i.MX25 Multimedia Applications Processor Reference Manual"(IMX25RM.pdf).
- 33.3.10 LCDC Panel Configuration Register (LPCR)
- 33.3.4 LCDC Screen Start Address Register (LSSAR)
And I found the relative information in the "Different Display Configurations on the i.MX25 WinCE PDK" (AN3977.pdf).
In this document, I could see that the LCDC didn't have the horizontal flip hardware acceleration, so 180 degree rotation can not be done by the LCDC.
So I want to perform the LCD 180 degree rotation or the Y-axis flip with the i.MX25 X-asix flip.
Could you tell me how to rotate the LCD 180 degree in i.MX25?
For Reference, I found the frame buffer rotation method by using OMAPpedia, but this method is not applied in the i.MX25.
For detailed information, refer to the below site.
[ Bootargs for enabling display ]
http://omappedia.org/wiki/Bootargs_for_enabling_display
~ $ echo "2" > /sys/class/graphics/fb0/rotate
Best Regards,
Eric.
已解决! 转到解答。
Hi Erik,
On i.MX25, It's only possible to flip along x-axis using HW. Other rotation/flip modes must be done by software (e.g. X11, QT, directfb and etc.
Rgds,
Rogerio