The L5.4.70_2.3.2 i.MX Linux release notes aka IMXLXRN wrongly states imx-dpu-g2d-6.4.3.p1.4.bin while the correct version is 1.8.14 (see https://source.codeaurora.org/external/imx/meta-imx/tree/meta-bsp/recipes-graphics/imx-dpu-g2d?h=zeu.... And BTW the following two also do not seem to exist:
imx-gpu-viv6.4.3.p1.4-aarch32.bin
imx-gpu-g2d-6.4.3.p1.4.bin
Hello
ok, the Release note is bad.
Regards