L5.4.3 BSP qca6174 compile faild

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

L5.4.3 BSP qca6174 compile faild

跳至解决方案
1,035 次查看
coindu
Contributor IV

Hi

      Build imx8mqevk image with L5.4.3 bsp, a error will appear about kernel-module-qcacld-lea on do_fetch stage.

     meta-imx\meta-bsp\recipes-kernel\kernel-modules\

      kernel-module-qcacld_3.1.inc

      kernel-module-qcacld-lea.inc

SRC_URI = "${QCACLD_SRC};branch=IMX_CNSS.LEA.NRT_3.0"
SRCREV = "7dc91e5977f31d60741c55682564788c0f930163"

 

     The branch and commit is not match, even if I change the branch name, it still compiles and reports errors.

      

coindu_0-1623380722818.png

coindu_1-1623380763997.png

 

 

    It seems that the BSP was not fully tested when it was released. 

 

     

标签 (1)
0 项奖励
回复
1 解答
1,024 次查看
jamesbone
NXP TechSupport
NXP TechSupport

The driver of the QCA6174 it is not longer available, since NXP already has their own Wifi Module, but you can contact the module maker or directly with Qualcomm in order to get a driver for the Linux BSP that you are using.  But it is not integrated in our BSP.  I apologize for the inconvenience.

 

 

 

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,025 次查看
jamesbone
NXP TechSupport
NXP TechSupport

The driver of the QCA6174 it is not longer available, since NXP already has their own Wifi Module, but you can contact the module maker or directly with Qualcomm in order to get a driver for the Linux BSP that you are using.  But it is not integrated in our BSP.  I apologize for the inconvenience.

 

 

 

0 项奖励
回复