L5.4.3 BSP qca6174 compile faild

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

L5.4.3 BSP qca6174 compile faild

ソリューションへジャンプ
1,034件の閲覧回数
coindu
Contributor IV

Hi

      Build imx8mqevk image with L5.4.3 bsp, a error will appear about kernel-module-qcacld-lea on do_fetch stage.

     meta-imx\meta-bsp\recipes-kernel\kernel-modules\

      kernel-module-qcacld_3.1.inc

      kernel-module-qcacld-lea.inc

SRC_URI = "${QCACLD_SRC};branch=IMX_CNSS.LEA.NRT_3.0"
SRCREV = "7dc91e5977f31d60741c55682564788c0f930163"

 

     The branch and commit is not match, even if I change the branch name, it still compiles and reports errors.

      

coindu_0-1623380722818.png

coindu_1-1623380763997.png

 

 

    It seems that the BSP was not fully tested when it was released. 

 

     

ラベル(1)
0 件の賞賛
返信
1 解決策
1,023件の閲覧回数
jamesbone
NXP TechSupport
NXP TechSupport

The driver of the QCA6174 it is not longer available, since NXP already has their own Wifi Module, but you can contact the module maker or directly with Qualcomm in order to get a driver for the Linux BSP that you are using.  But it is not integrated in our BSP.  I apologize for the inconvenience.

 

 

 

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,024件の閲覧回数
jamesbone
NXP TechSupport
NXP TechSupport

The driver of the QCA6174 it is not longer available, since NXP already has their own Wifi Module, but you can contact the module maker or directly with Qualcomm in order to get a driver for the Linux BSP that you are using.  But it is not integrated in our BSP.  I apologize for the inconvenience.

 

 

 

0 件の賞賛
返信