L5.10.9, there's no mxc_iomux_v3_setup_multiple_pads

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

L5.10.9, there's no mxc_iomux_v3_setup_multiple_pads

867 Views
TKayO
Contributor III

Hello, 

I cannot find mxc_iomux_v3_setup_multiple_pads in Kernel 5.10.9, Yocto BSP

I'd like to know the beginning of architecture change and 

how can I do the same thing in 5.10?

 

Regards.

 

Tags (1)
0 Kudos
Reply
1 Reply

857 Views
joanxie
NXP TechSupport
NXP TechSupport

what beginning of architecture change do you mean? could you give me an example in the old bsp?

I don't know what board you are talking about, if you mean imx6q, maybe you can refer to:

"https://source.codeaurora.org/external/imx/linux-imx/tree/arch/arm/mach-imx/mach-imx6q.c?h=lf-5.10.y...

focus on the function "imx6q_init_machine"

0 Kudos
Reply