L4.1.15_2.0.0 cook mfgtools like below command show,
bitbake fsl-image-mfgtool-initramfs
got two ERRORS, then what can i do? thanks.
ERROR: mfgtool-linux-imx-4.1.15-r0 do_package: Taskhash mismatch 08f424ded43e62e094a609f24d138620 verses 5136119db6285fc41c1d6fa4bd0bd663 for /home/jaloo/backup/sabre/yocto/src/L4.1.15_2.0.0/fsl-release-bsp/sources/meta-fsl-bsp-release/imx/meta-bsp/recipes-kernel/linux/linux-imx-mfgtool_4.1.15.bb.do_package
ERROR: Taskhash mismatch 08f424ded43e62e094a609f24d138620 verses 5136119db6285fc41c1d6fa4bd0bd663 for /home/jaloo/backup/sabre/yocto/src/L4.1.15_2.0.0/fsl-release-bsp/sources/meta-fsl-bsp-release/imx/meta-bsp/recipes-kernel/linux/linux-imx-mfgtool_4.1.15.bb.do_package
Hi 家禄 刘
for "mismatch" errors workaround please refer to
sect.6.2 Manufacturing Tool, MFGTool attached Yocto Guide:
"In krogoth release there are sometimes task hask mismatch errors.
A fix for this is to build linux-imx first then clean the
linux-mfgtools then bitbake the fsl-image-mfgtool-initramfs."
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------