L4.1.15_2.0.0 cook mfgtools got two errors

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

L4.1.15_2.0.0 cook mfgtools got two errors

599 Views
liu_jialu
Contributor III

L4.1.15_2.0.0 cook mfgtools like below command show,

              bitbake fsl-image-mfgtool-initramfs

got two ERRORS, then what can i do? thanks.

ERROR: mfgtool-linux-imx-4.1.15-r0 do_package: Taskhash mismatch 08f424ded43e62e094a609f24d138620 verses 5136119db6285fc41c1d6fa4bd0bd663 for /home/jaloo/backup/sabre/yocto/src/L4.1.15_2.0.0/fsl-release-bsp/sources/meta-fsl-bsp-release/imx/meta-bsp/recipes-kernel/linux/linux-imx-mfgtool_4.1.15.bb.do_package
ERROR: Taskhash mismatch 08f424ded43e62e094a609f24d138620 verses 5136119db6285fc41c1d6fa4bd0bd663 for /home/jaloo/backup/sabre/yocto/src/L4.1.15_2.0.0/fsl-release-bsp/sources/meta-fsl-bsp-release/imx/meta-bsp/recipes-kernel/linux/linux-imx-mfgtool_4.1.15.bb.do_package

Labels (3)
0 Kudos
1 Reply

335 Views
igorpadykov
NXP Employee
NXP Employee

Hi 家禄 刘 

for "mismatch" errors workaround please refer to

sect.6.2 Manufacturing Tool, MFGTool attached Yocto Guide:

"In krogoth release there are sometimes task hask mismatch errors.

A fix for this is to build linux-imx first then clean the
linux-mfgtools then bitbake the fsl-image-mfgtool-initramfs."

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos