Hi all,
I have a sabre automotive i.mx6q board. I installed yocto linux into it.
How can I use keyboard/mouse with it ? When I try to logitech M235 wireless mouse the board can't detect it.
Also which usb port I can use for Keyboard/Mouse ?
Thank you from now.
I don't have the source code is there a way to change it from OS ? I will try the cable soon.
Are'nt you having the source code of the Sabre Auto?
Try with the cable shown by Dan Wang.
Is this file avaliable before -make all command in buildroot or it is already in OS after install?
Atm there isn't such a directory in OS. We are using yocto/open embedded atm. And I have the finalized image only. My file directory in board looks like this:
bin lost+found proc tmp
boot home media run unit_tests
dev mnt sbin usr
etc lib opt sys var
I tried both with mouse and keyboard but it wasn't with the otg to usb 2.0 cable it was with the connector that i posted above.
When i measure the output of otg, is is between 0.2 - 03 mV
In your kernel directory,go to arch/arm/boot/dts . In this location you will get all the device tree related files. Search for imx6qdl-sabreauto.dtsi.
Also have you tried connecting mouse? Is the board able to give power to it?
Hi,
Where I can find that file ?
Hi
Yes it can be one issue you need to enable the power for usb otg vbus.Can you show me your imx6qdl-sabreauto.dtsi configuration?
hi all,
Also output of usb otg is near 0V I get this message from dmesg or on boot loading.
ci_hdrc ci_hdrc.1: new USB bus registered, assigned bus number 1
ci_hdrc ci_hdrc.1: USB 2.0 started, EHCI 1.00
hub 1-0:1.0: USB hub found
hub 1-0:1.0: 1 port detected
input: gpio-keys as /devices/soc0/gpio-keys/input/input4
snvs_rtc 20cc000.snvs:snvs-rtc-lp: setting system clock to 2016-07-14 12:32:19 UTC (1468499539)
can-stby: disabling
can-en: disabling
usb_otg_vbus: disabling => can it be the problem ?
Hi
You can use the OTG port as shown in the figure.You need to use OTG to USB 2.0 cable to connect your mouse/keyboard
Thank you or reply, I am using this connection. Can it be the cause of problem?
Hi,
Yes. Here you can use otg line to connect the keyboard or mouse to your board.
Have a great day,
Dan
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Mark Correct button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi
I am not able to view the image.Can you repost it.
Here is the image:
You can use the cable shown by Dan Wang