Hello all,
I am just beginning to work at creating a yocto environment for a new device which uses the var-som-6ul module. Our device requires the use of kexec.
I compiled a custom kernel and was able to boot that kernel from u-boot. Everything was fine.
But when attempting to use kexec to boot back into the same kernel, I got the following boot message:
kexec -d -l /mnt/images/boot/zImage --dtb /mnt/images/boot/imx6ull-var-som-concerto-board-nand-sd
-card.dtb '--append=root=/dev/ram0 console=ttymxc0,115200 rootwait=1 rw earlyprintk '
syscall kexec_file_load not available.
Try gzip decompression.
Try LZMA decompression.
lzma_decompress_file: read on /mnt/images/boot/zImage of 2127437444 bytes failed
kernel: 0x76599008 kernel_size: 0x805c70
MEMORY RANGES
0000000080000000-000000009fffffff (0)
zImage header: 0x016f2818 0x00000000 0x00805c70
zImage size 0x805c70, file size 0x805c70
zImage requires 0x00816c70 bytes
offset 0x00001980 tag 0x5a534c4b size 8
Decompressed kernel sizes:
text+data 0x012b1d80 bss 0x0006c568 total 0x0131e2e8
Resulting kernel space: 0x01ac89f0
Kernel: address=0x80008000 size=0x01ac89f0
DT : address=0x81ad2000 size=0x00008600
kexec_load: entry = 0x80008000 flags = 0x280000
nr_segments = 2
segment[0].buf = 0x76599008
segment[0].bufsz = 0x805c74
segment[0].mem = 0x80008000
segment[0].memsz = 0x806000
segment[1].buf = 0xd58658
segment[1].bufsz = 0x8600
segment[1].mem = 0x81ad2000
segment[1].memsz = 0x9000
+ kexec -e
[ 40.810290] cfg80211: failed to load regulatory.db
[ 40.848865] ci_hdrc ci_hdrc.1: remove, state 4
[ 40.854702] usb usb1: USB disconnect, device number 1
[ 40.870996] ci_hdrc ci_hdrc.1: USB bus 1 deregistered
[ 40.894760] kexec_core: Starting new kernel
[ 40.912538] Disabling non-boot CPUs ...
[ 40.919907] Bye!
[ 0.000000] Booting Linux on physical CPU 0x0
[ 0.000000] Linux version 5.4.3-imx6ul+gb40ccfdb73ea (oe-user@oe-host) (gcc version 9.2.0 (GCC))
#1 SMP PREEMPT Sat Jan 2 20:29:17 UTC 2021
[ 0.000000] CPU: ARMv7 Processor [410fc075] revision 5 (ARMv7), cr=10c5387d
[ 0.000000] CPU: div instructions available: patching division code
[ 0.000000] CPU: PIPT / VIPT nonaliasing data cache, VIPT aliasing instruction cache
[ 0.000000] OF: fdt: Machine model: Variscite VAR-SOM-6UL with i.MX6ULL, NAND flash & SD card su
pport on Concerto-Board
[ 0.000000] printk: bootconsole [earlycon0] enabled
[ 0.000000] Memory policy: Data cache writealloc
[ 0.000000] cma: Size (0x02000000) of region at 0x00000000 exceeds limit (0x00000000)
[ 0.000000] cma: Failed to reserve 32 MiB
[ 0.000000] Kernel panic - not syncing: early_alloc: Failed to allocate 8192 bytes align=0x2000
[ 0.000000] ---[ end Kernel panic - not syncing: early_alloc: Failed to allocate 8192 bytes alig
n=0x2000 ]---
So somehow the u-boot environment is different from the kexec environment in terms of the memory, it seems.
In the past, I have been able to fix this problem by either a linux command line option: (mem=xxxx??)
or in the device tree.
But after experimenting with both of those approaches, I have had no success.
Has anyone had any experience with this and could help?
Thanks,
Brian