Kernel started up but stuck

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Kernel started up but stuck

2,327 Views
hexiaojun3
Contributor II

Hi expert,

My system log dumps is below, the issue is the console is stuck after kernel startup, I cannot enter any key. It seems not be redirect to ttymxc2 successfully. 

I had a test and can verify the ethernet is ok, can telnet my board from my labtop.

And UART pinctrl settings should be no confliction for NXP official EVM is adopted UART1 and UART3 interfaces already.

Would you please take a look and give me a hint what's the root cause probably? 

thanks,

Xiaojun

U-Boot 2015.04 (Sep 05 2024 - 03:04:47)

CPU: Freescale i.MX6Q rev1.6 at 792 MHz
CPU: Temperature 24 C
Reset cause: POR
Board: MX6-SabreSD
I2C: ready
DRAM: 2 GiB
MMC: FSL_SDHC: 0, FSL_SDHC: 1, FSL_SDHC: 2
LCD type:7.0
bootsystem:qt
bootargs=console=ttymxc2,115200 androidboot.console=ttymxc2 consoleblank=0 vmalloc=256M video=mxcfb0:dev=ldb,VGA_8001280 video=mxcfb1:off video=mxcfb2:off video=mxcfb3:off root=/dev/mmcblk2p5 rootwait rw
Display: 7.0 (800x1280)
In: serial
Out: serial
Err: serial
switch to partitions #0, OK
mmc1 is current device
Net: Phy 0 not found
PHY reset timed out
FEC [PRIME]
Normal Boot
Hit any key to stop autoboot: 0
reading topeet_7inch.dtb
46753 bytes read in 19 ms (2.3 MiB/s)
reading zImage
8522560 bytes read in 403 ms (20.2 MiB/s)
Kernel image @ 0x13000000 [ 0x000000 - 0x820b40 ]
## Flattened Device Tree blob at 12000000
Booting using the fdt blob at 0x12000000
Using Device Tree in place at 12000000, end 1200e6a0
No PMIC found!

Starting kernel ...

Booting Linux on physical CPU 0x0
Initializing cgroup subsys cpu
Initializing cgroup subsys cpuacct
Linux version 4.1.15 (topeet@ubuntu) (gcc version 4.9.x-google 20140827 (prerelease) (GCC) ) #10 SMP PREEMPT Thu Sep 19 20:38:37 PDT 2024
CPU: ARMv7 Processor [412fc09a] revision 10 (ARMv7), cr=10c53c7d
CPU: PIPT / VIPT nonaliasing data cache, VIPT aliasing instruction cache
Machine model: Freescale i.MX6 Quad SABRE Smart Device Board
Memory policy: Data cache writealloc
PERCPU: Embedded 365 pages/cpu @ed9fb000 s1465664 r8192 d21184 u1495040
Built 1 zonelists in Zone order, mobility grouping on. Total pages: 522528
Kernel command line: console=ttymxc2,115200 androidboot.console=ttymxc2 consoleblank=0 vmalloc=256M video=mxcfb0:dev=ldb,VGA_8001280 video=mxcfb1:off video=mxcfb2:off video=mxcfb3:off root=/dev/mmcblk2p5 rootwait rw
PID hash table entries: 4096 (order: 2, 16384 bytes)
Dentry cache hash table entries: 131072 (order: 7, 524288 bytes)
Inode-cache hash table entries: 65536 (order: 6, 262144 bytes)
Memory: 2044588K/2096128K available (12570K kernel code, 842K rwdata, 3416K rodata, 2048K init, 8876K bss, 51540K reserved, 0K cma-reserved, 1326080K highmem)
Virtual kernel memory layout:
vector : 0xffff0000 - 0xffff1000 ( 4 kB)
fixmap : 0xffc00000 - 0xfff00000 (3072 kB)
vmalloc : 0xef800000 - 0xff000000 ( 248 MB)
lowmem : 0xc0000000 - 0xef000000 ( 752 MB)
pkmap : 0xbfe00000 - 0xc0000000 ( 2 MB)
modules : 0xbf000000 - 0xbfe00000 ( 14 MB)
.text : 0xc0008000 - 0xc109c920 (16979 kB)
.init : 0xc1100000 - 0xc1300000 (2048 kB)
.data : 0xc1300000 - 0xc13d2968 ( 843 kB)
.bss : 0xc13d2968 - 0xc1c7db30 (8877 kB)
SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=4, Nodes=1
Running RCU self tests
Preemptible hierarchical RCU implementation.
RCU lockdep checking is enabled.
Additional per-CPU info printed with stalls.
NR_IRQS:16 nr_irqs:16 16
L2C-310 erratum 769419 enabled
L2C-310 enabling early BRESP for Cortex-A9
L2C-310 full line of zeros enabled for Cortex-A9
L2C-310 ID prefetch enabled, offset 16 lines
L2C-310 dynamic clock gating enabled, standby mode enabled
L2C-310 cache controller enabled, 16 ways, 1024 kB
L2C-310: CACHE_ID 0x410000c7, AUX_CTRL 0x76070001
mxc_clocksource_init 3000000
Switching to timer-based delay loop, resolution 333ns
sched_clock: 32 bits at 3000kHz, resolution 333ns, wraps every 715827882841ns
clocksource mxc_timer1: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 637086815595 ns
Console: colour dummy device 80x30
Lock dependency validator: Copyright (c) 2006 Red Hat, Inc., Ingo Molnar
... MAX_LOCKDEP_SUBCLASSES: 8
... MAX_LOCK_DEPTH: 48
... MAX_LOCKDEP_KEYS: 8191
... CLASSHASH_SIZE: 4096
... MAX_LOCKDEP_ENTRIES: 32768
... MAX_LOCKDEP_CHAINS: 65536
... CHAINHASH_SIZE: 32768
memory used by lock dependency info: 5423 kB
per task-struct memory footprint: 2304 bytes
------------------------
| Locking API testsuite:
----------------------------------------------------------------------------
| spin |wlock |rlock |mutex | wsem | rsem |
--------------------------------------------------------------------------
A-A deadlock: ok | ok | ok | ok |
unwind: Unknown symbol address c01014a4
unwind: Index not found c01014a4
unwind: Unknown symbol address c01014a4
unwind: Index not found c01014a4
unwind: Unknown symbol address c01014a4
unwind: Index not found c01014a4
unwind: Unknown symbol address c01014a4
unwind: Index not found c01014a4
unwind: Unknown symbol address c01014a4
unwind: Index not found c01014a4
unwind: Unknown symbol address c01014a4
unwind: Index not found c01014a4
unwind: Unknown symbol address c01014a4
unwind: Index not found c01014a4
unwind: Unknown symbol address c01014a4
unwind: Index not found c01014a4
unwind: Unknown symbol address c01014a4
unwind: Index not found c01014a4
unwind: Unknown symbol address c01014a4
unwind: Index not found c01014a4
unwind: Unknown symbol address c01014a4
unwind: Index not found c01014a4
unwind: Unknown symbol address c01014a4
unwind: Index not found c01014a4
unwind: Unknown symbol address c01014a4
unwind: Index not found c01014a4
ok | ok |
A-B-B-A deadlock: ok | ok | ok | ok | ok | ok |
A-B-B-C-C-A deadlock: ok | ok | ok | ok | ok | ok |
A-B-C-A-B-C deadlock: ok | ok | ok | ok | ok | ok |
A-B-B-C-C-D-D-A deadlock: ok | ok | ok | ok | ok | ok |
A-B-C-D-B-D-D-A deadlock: ok | ok | ok | ok | ok | ok |
A-B-C-D-B-C-D-A deadlock: ok | ok | ok | ok | ok | ok |
double unlock: ok | ok | ok | ok | ok | ok |
initialize held: ok | ok | ok | ok | ok | ok |
bad unlock order: ok | ok | ok | ok | ok | ok |
--------------------------------------------------------------------------
recursive read-lock: | ok | | ok |
recursive read-lock #2: | ok | | ok |
mixed read-write-lock: | ok | | ok |
mixed write-read-lock: | ok | | ok |
--------------------------------------------------------------------------
hard-irqs-on + irq-safe-A/12: ok | ok | ok |
soft-irqs-on + irq-safe-A/12: ok | ok | ok |
hard-irqs-on + irq-safe-A/21: ok | ok | ok |
soft-irqs-on + irq-safe-A/21: ok | ok | ok |
sirq-safe-A => hirqs-on/12: ok | ok | ok |
sirq-safe-A => hirqs-on/21: ok | ok | ok |
hard-safe-A + irqs-on/12: ok | ok | ok |
soft-safe-A + irqs-on/12: ok | ok | ok |
hard-safe-A + irqs-on/21: ok | ok | ok |
soft-safe-A + irqs-on/21: ok | ok | ok |
hard-safe-A + unsafe-B #1/123: ok | ok | ok |
soft-safe-A + unsafe-B #1/123: ok | ok | ok |
hard-safe-A + unsafe-B #1/132: ok | ok | ok |
soft-safe-A + unsafe-B #1/132: ok | ok | ok |
hard-safe-A + unsafe-B #1/213: ok | ok | ok |
soft-safe-A + unsafe-B #1/213: ok | ok | ok |
hard-safe-A + unsafe-B #1/231: ok | ok | ok |
soft-safe-A + unsafe-B #1/231: ok | ok | ok |
hard-safe-A + unsafe-B #1/312: ok | ok | ok |
soft-safe-A + unsafe-B #1/312: ok | ok | ok |
hard-safe-A + unsafe-B #1/321: ok | ok | ok |
soft-safe-A + unsafe-B #1/321: ok | ok | ok |
hard-safe-A + unsafe-B #2/123: ok | ok | ok |
soft-safe-A + unsafe-B #2/123: ok | ok | ok |
hard-safe-A + unsafe-B #2/132: ok | ok | ok |
soft-safe-A + unsafe-B #2/132: ok | ok | ok |
hard-safe-A + unsafe-B #2/213: ok | ok | ok |
soft-safe-A + unsafe-B #2/213: ok | ok | ok |
hard-safe-A + unsafe-B #2/231: ok | ok | ok |
soft-safe-A + unsafe-B #2/231: ok | ok | ok |
hard-safe-A + unsafe-B #2/312: ok | ok | ok |
soft-safe-A + unsafe-B #2/312: ok | ok | ok |
hard-safe-A + unsafe-B #2/321: ok | ok | ok |
soft-safe-A + unsafe-B #2/321: ok | ok | ok |
hard-irq lock-inversion/123: ok | ok | ok |
soft-irq lock-inversion/123: ok | ok | ok |
hard-irq lock-inversion/132: ok | ok | ok |
soft-irq lock-inversion/132: ok | ok | ok |
hard-irq lock-inversion/213: ok | ok | ok |
soft-irq lock-inversion/213: ok | ok | ok |
hard-irq lock-inversion/231: ok | ok | ok |
soft-irq lock-inversion/231: ok | ok | ok |
hard-irq lock-inversion/312: ok | ok | ok |
soft-irq lock-inversion/312: ok | ok | ok |
hard-irq lock-inversion/321: ok | ok | ok |
soft-irq lock-inversion/321: ok | ok | ok |
hard-irq read-recursion/123: ok |
soft-irq read-recursion/123: ok |
hard-irq read-recursion/132: ok |
soft-irq read-recursion/132: ok |
hard-irq read-recursion/213: ok |
soft-irq read-recursion/213: ok |
hard-irq read-recursion/231: ok |
soft-irq read-recursion/231: ok |
hard-irq read-recursion/312: ok |
soft-irq read-recursion/312: ok |
hard-irq read-recursion/321: ok |
soft-irq read-recursion/321: ok |
--------------------------------------------------------------------------
| Wound/wait tests |
---------------------
ww api failures: ok | ok | ok |
ww contexts mixing: ok | ok |
finishing ww context: ok | ok | ok | ok |
locking mismatches: ok | ok | ok |
EDEADLK handling: ok | ok | ok | ok | ok | ok | ok | ok | ok | ok |
spinlock nest unlocked: ok |
-----------------------------------------------------
|block | try |context|
-----------------------------------------------------
context: ok | ok | ok |
try: ok | ok | ok |
block: ok | ok | ok |
spinlock: ok | ok | ok |
-------------------------------------------------------
Good, all 253 testcases passed! |
---------------------------------
Calibrating delay loop (skipped), value calculated using timer frequency.. 6.00 BogoMIPS (lpj=30000)
pid_max: default: 32768 minimum: 301
Mount-cache hash table entries: 2048 (order: 1, 8192 bytes)
Mountpoint-cache hash table entries: 2048 (order: 1, 8192 bytes)
Initializing cgroup subsys freezer
Initializing cgroup subsys debug
CPU: Testing write buffer coherency: ok
CPU0: thread -1, cpu 0, socket 0, mpidr 80000000
Setting up static identity map for 0x10100000 - 0x10100058
unwind: Unknown symbol address c01014a4
unwind: Index not found c01014a4
CPU1: thread -1, cpu 1, socket 0, mpidr 80000001
CPU2: thread -1, cpu 2, socket 0, mpidr 80000002
CPU3: thread -1, cpu 3, socket 0, mpidr 80000003
Brought up 4 CPUs
SMP: Total of 4 processors activated (24.00 BogoMIPS).
CPU: All CPU(s) started in SVC mode.
devtmpfs: initialized
unwind: Unknown symbol address c01014a4
unwind: Index not found c01014a4
VFP support v0.3: implementor 41 architecture 3 part 30 variant 9 rev 4
clocksource jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 19112604462750000 ns
pinctrl core: initialized pinctrl subsystem
NET: Registered protocol family 16
DMA: preallocated 256 KiB pool for atomic coherent allocations
unwind: Unknown symbol address c01014a4
unwind: Index not found c01014a4
unwind: Unknown symbol address c01014a4
unwind: Index not found c01014a4
unwind: Unknown symbol address c01014a4
unwind: Index not found c01014a4
unwind: Unknown symbol address c01014a4
unwind: Index not found c01014a4
unwind: Unknown symbol address c01014a4
unwind: Index not found c01014a4
unwind: Unknown symbol address c01014a4
unwind: Index not found c01014a4
unwind: Unknown symbol address c01014a4
unwind: Index not found c01014a4
unwind: Unknown symbol address c01014a4
unwind: Index not found c01014a4
unwind: Unknown symbol address c01014a4
unwind: Index not found c01014a4
unwind: Unknown symbol address c01014a4
unwind: Index not found c01014a4
cpuidle: using governor ladder
cpuidle: using governor menu
CPU identified as i.MX6Q, silicon rev 0.6
!!request miniPCIE Power On gpio
hw-breakpoint: found 5 (+1 reserved) breakpoint and 1 watchpoint registers.
hw-breakpoint: maximum watchpoint size is 4 bytes.
VDSO is not a valid ELF object!
imx6q-pinctrl 20e0000.iomuxc: Invalid fsl,pins property in node /soc/aips-bus@02000000/iomuxc@020e0000/imx6qdl-sabresd/ecspi1grp
imx6q-pinctrl 20e0000.iomuxc: Invalid fsl,pins property in node /soc/aips-bus@02000000/iomuxc@020e0000/imx6qdl-sabresd/hdmihdcpgrp
imx6q-pinctrl 20e0000.iomuxc: Invalid fsl,pins property in node /soc/aips-bus@02000000/iomuxc@020e0000/imx6qdl-sabresd/i2c2grp
imx6q-pinctrl 20e0000.iomuxc: initialized IMX pinctrl driver
mxs-dma 110000.dma-apbh: initialized
MPCIE_3V3: Failed to request enable GPIO83: -16
reg-fixed-voltage regulators:regulator@3: Failed to register regulator: -16
reg-fixed-voltage: probe of regulators:regulator@3 failed with error -16
vgaarb: loaded
SCSI subsystem initialized
usbcore: registered new interface driver usbfs
usbcore: registered new interface driver hub
usbcore: registered new device driver usb
2000000.aips-bus:usbphy_nop1 supply vcc not found, using dummy regulator
2000000.aips-bus:usbphy_nop2 supply vcc not found, using dummy regulator
i2c i2c-0: IMX I2C adapter registered
i2c i2c-0: can't use DMA
i2c i2c-2: IMX I2C adapter registered
i2c i2c-2: can't use DMA
pps_core: LinuxPPS API ver. 1 registered
pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <[email protected]>
PTP clock support registered
imx-ipuv3 2400000.ipu: IPU DMFC NORMAL mode: 1(0~1), 5B(4,5), 5F(6,7)
unwind: Unknown symbol address c01014a4
unwind: Index not found c01014a4
imx-ipuv3 2800000.ipu: IPU DMFC NORMAL mode: 1(0~1), 5B(4,5), 5F(6,7)
mxc_mipi_csi2 21dc000.mipi_csi: i.MX MIPI CSI2 driver probed
mxc_mipi_csi2 21dc000.mipi_csi: i.MX MIPI CSI2 dphy version is 0x3130302a
MIPI CSI2 driver module loaded
Advanced Linux Sound Architecture Driver Initialized.
Bluetooth: Core ver 2.20
NET: Registered protocol family 31
Bluetooth: HCI device and connection manager initialized
Bluetooth: HCI socket layer initialized
Bluetooth: L2CAP socket layer initialized
Bluetooth: SCO socket layer initialized
Switched to clocksource mxc_timer1
unwind: Unknown symbol address c01014a4
unwind: Index not found c01014a4
unwind: Unknown symbol address c01014a4
unwind: Index not found c01014a4
unwind: Unknown symbol address c01014a4
unwind: Index not found c01014a4
unwind: Unknown symbol address c01014a4
unwind: Index not found c01014a4
unwind: Unknown symbol address c01014a4
unwind: Index not found c01014a4
unwind: Unknown symbol address c01014a4
unwind: Index not found c01014a4
unwind: Unknown symbol address c01014a4
unwind: Index not found c01014a4
unwind: Unknown symbol address c01014a4
unwind: Index not found c01014a4
unwind: Unknown symbol address c01014a4
unwind: Index not found c01014a4
unwind: Unknown symbol address c01014a4
unwind: Index not found c01014a4
unwind: Unknown symbol address c01014a4
unwind: Index not found c01014a4
unwind: Unknown symbol address c01014a4
unwind: Index not found c01014a4
unwind: Unknown symbol address c01014a4
unwind: Index not found c01014a4
NET: Registered protocol family 2
TCP established hash table entries: 8192 (order: 3, 32768 bytes)
unwind: Unknown symbol address c01014a4
unwind: Index not found c01014a4
TCP bind hash table entries: 8192 (order: 6, 360448 bytes)
TCP: Hash tables configured (established 8192 bind 8192)
UDP hash table entries: 512 (order: 3, 49152 bytes)
UDP-Lite hash table entries: 512 (order: 3, 49152 bytes)
NET: Registered protocol family 1
RPC: Registered named UNIX socket transport module.
RPC: Registered udp transport module.
RPC: Registered tcp transport module.
RPC: Registered tcp NFSv4.1 backchannel transport module.
unwind: Unknown symbol address c01014a4
unwind: Index not found c01014a4
CPU PMU: Failed to parse /soc/pmu/interrupt-affinity[0]
hw perfevents: enabled with armv7_cortex_a9 PMU driver, 7 counters available
imx rpmsg driver is registered.
Bus freq driver module loaded
console [pstore-1] enabled
pstore: Registered ramoops as persistent store backend
ramoops: attached 0x100000@0x8bf00000, ecc: 0/0
mxc_ramoops device success loaded
futex hash table entries: 1024 (order: 4, 65536 bytes)
audit: initializing netlink subsys (disabled)
audit: type=2000 audit(1.750:1): initialized
unwind: Unknown symbol address c01014a4
unwind: Index not found c01014a4
unwind: Unknown symbol address c01014a4
unwind: Index not found c01014a4
unwind: Unknown symbol address c01014a4
unwind: Index not found c01014a4
unwind: Unknown symbol address c01014a4
unwind: Index not found c01014a4
unwind: Unknown symbol address c01014a4
unwind: Index not found c01014a4
VFS: Disk quotas dquot_6.6.0
VFS: Dquot-cache hash table entries: 1024 (order 0, 4096 bytes)
NFS: Registering the id_resolver key type
Key type id_resolver registered
Key type id_legacy registered
ntfs: driver 2.1.32 [Flags: R/W DEBUG].
jffs2: version 2.2. (NAND) ? 2001-2006 Red Hat, Inc.
fuse init (API version 7.23)
bounce: pool size: 64 pages
io scheduler noop registered
io scheduler deadline registered
io scheduler cfq registered (default)
imx-weim 21b8000.weim: Driver registered.
mxc_mipi_dsi 21e0000.mipi: i.MX MIPI DSI driver probed
MIPI DSI driver module loaded
MIPI DSI driver module loaded
mxc_sdc_fb fb@0: registered mxc display driver ldb
unwind: Unknown symbol address c01014a4
unwind: Index not found c01014a4
unwind: Unknown symbol address c01014a4
unwind: Index not found c01014a4
unwind: Unknown symbol address c01014a4
unwind: Index not found c01014a4
unwind: Unknown symbol address c01014a4
unwind: Index not found c01014a4
unwind: Unknown symbol address c01014a4
unwind: Index not found c01014a4
Console: switching to colour frame buffer device 100x80
unwind: Unknown symbol address c01014a4
unwind: Index not found c01014a4
unwind: Unknown symbol address c01014a4
unwind: Index not found c01014a4
unwind: Unknown symbol address c01014a4
unwind: Index not found c01014a4
unwind: Unknown symbol address c01014a4
unwind: Index not found c01014a4
mxc_sdc_fb fb@1: Can't get fb option for mxcfb1!
mxc_sdc_fb fb@2: Can't get fb option for mxcfb2!
mxc_sdc_fb fb@3: Can't get fb option for mxcfb3!
imx-sdma 20ec000.sdma: no iram assigned, using external mem
imx-sdma 20ec000.sdma: no event needs to be remapped
imx-sdma 20ec000.sdma: loaded firmware 3.3
imx-sdma 20ec000.sdma: initialized
2020000.serial: ttymxc0 at MMIO 0x2020000 (irq = 23, base_baud = 5000000) is a IMX
21e8000.serial: ttymxc1 at MMIO 0x21e8000 (irq = 299, base_baud = 5000000) is a IMX
21ec000.serial: ttymxc2 at MMIO 0x21ec000 (irq = 300, base_baud = 5000000) is a IMX
unwind: Unknown symbol address c01014a4
unwind: Index not found c01014a4
unwind: Unknown symbol address c01014a4
unwind: Index not found c01014a4
unwind: Unknown symbol address c01014a4
unwind: Index not found c01014a4
unwind: Unknown symbol address c01014a4
unwind: Index not found c01014a4
unwind: Unknown symbol address c01014a4
unwind: Index not found c01014a4
unwind: Unknown symbol address c01014a4
unwind: Index not found c01014a4
unwind: Unknown symbol address c01014a4
unwind: Index not found c01014a4
unwind: Unknown symbol address c01014a4
unwind: Index not found c01014a4
console [ttymxc2] enabled
imx sema4 driver is registered.
[drm] Initialized drm 1.1.0 20060810
[drm] Initialized vivante 1.0.0 20120216 on minor 0
brd: module loaded
loop: module loaded
zram: Created 1 device(s)
tun: Universal TUN/TAP device driver, 1.6
tun: (C) 1999-2004 Max Krasnyansky <[email protected]>
CAN device driver interface
flexcan 2090000.flexcan: device registered (reg_base=efe80000, irq=29)
2188000.ethernet supply phy not found, using dummy regulator
unwind: Unknown symbol address c01014a4
unwind: Index not found c01014a4
unwind: Unknown symbol address c01014a4
unwind: Index not found c01014a4
unwind: Unknown symbol address c01014a4
unwind: Index not found c01014a4
pps pps0: new PPS source ptp0
unwind: Unknown symbol address c01014a4
unwind: Index not found c01014a4
unwind: Unknown symbol address c01014a4
unwind: Index not found c01014a4
unwind: Unknown symbol address c01014a4
unwind: Index not found c01014a4
unwind: Unknown symbol address c01014a4
unwind: Index not found c01014a4
unwind: Unknown symbol address c01014a4
unwind: Index not found c01014a4
libphy: fec_enet_mii_bus: probed
fec 2188000.ethernet eth0: registered PHC device 0
PPP generic driver version 2.4.2
PPP BSD Compression module registered
PPP Deflate Compression module registered
PPP MPPE Compression module registered
NET: Registered protocol family 24
unwind: Unknown symbol address c01014a4
unwind: Index not found c01014a4
unwind: Unknown symbol address c01014a4
unwind: Index not found c01014a4
unwind: Unknown symbol address c01014a4
unwind: Index not found c01014a4
pegasus: v0.9.3 (2013/04/25), Pegasus/Pegasus II USB Ethernet driver
usbcore: registered new interface driver pegasus
usbcore: registered new interface driver rtl8150
usbcore: registered new interface driver r8152
usbcore: registered new interface driver asix
usbcore: registered new interface driver ax88179_178a
usbcore: registered new interface driver cdc_ether
usbcore: registered new interface driver cdc_eem
usbcore: registered new interface driver dm9601
usbcore: registered new interface driver net1080
usbcore: registered new interface driver cdc_subset
usbcore: registered new interface driver zaurus
usbcore: registered new interface driver cdc_ncm
ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver
ehci-pci: EHCI PCI platform driver
ehci-mxc: Freescale On-Chip EHCI Host driver
ohci_hcd: USB 1.1 'Open' Host Controller (OHCI) Driver
ohci-pci: OHCI PCI platform driver
ohci-platform: OHCI generic platform driver
usbcore: registered new interface driver cdc_acm
cdc_acm: USB Abstract Control Model driver for USB modems and ISDN adapters
usbcore: registered new interface driver usb-storage
usbcore: registered new interface driver usbserial
usbcore: registered new interface driver usbserial_generic
usbserial: USB Serial support registered for generic
usbcore: registered new interface driver ftdi_sio
usbserial: USB Serial support registered for FTDI USB Serial Device
usbcore: registered new interface driver option
usbserial: USB Serial support registered for GSM modem (1-port)
usbcore: registered new interface driver usb_ehset_test
2184800.usbmisc supply vbus-wakeup not found, using dummy regulator
2184200.usb supply vbus not found, using dummy regulator
ci_hdrc ci_hdrc.1: EHCI Host Controller
ci_hdrc ci_hdrc.1: new USB bus registered, assigned bus number 1
ci_hdrc ci_hdrc.1: USB 2.0 started, EHCI 1.00
usb usb1: New USB device found, idVendor=1d6b, idProduct=0002
usb usb1: New USB device strings: Mfr=3, Product=2, SerialNumber=1
usb usb1: Product: EHCI Host Controller
usb usb1: Manufacturer: Linux 4.1.15 ehci_hcd
usb usb1: SerialNumber: ci_hdrc.1
hub 1-0:1.0: USB hub found
hub 1-0:1.0: 1 port detected
i2c /dev entries driver
imx2-wdt 20bc000.wdog: timeout 60 sec (nowayout=0)
Bluetooth: HCI UART driver ver 2.3
Bluetooth: HCI UART protocol H4 registered
Bluetooth: HCI UART protocol BCSP registered
Bluetooth: HCI UART protocol ATH3K registered
usbcore: registered new interface driver btusb
rtk_btusb: Realtek Bluetooth USB driver module init, version 4.0.2
rtk_btusb: Register usb char device interface for BT driver
usbcore: registered new interface driver rtk_btusb
sdhci: Secure Digital Host Controller Interface driver
sdhci: Copyright(c) Pierre Ossman
sdhci-pltfm: SDHCI platform and OF driver helper
BUG: sleeping function called from invalid context at kernel/locking/mutex.c:616
in_atomic(): 1, irqs_disabled(): 0, pid: 1, name: swapper/0
3 locks held by swapper/0/1:
#0: (&dev->mutex){......}, at: [<c061aa58>] __driver_attach+0x48/0x98
#1: (&dev->mutex){......}, at: [<c061aa68>] __driver_attach+0x58/0x98
#2: (mmc_host_lock){+.+...}, at: [<c07b5258>] mmc_alloc_host+0x3c/0x238
Preemption disabled at:[< (null)>] (null)

CPU: 2 PID: 1 Comm: swapper/0 Not tainted 4.1.15 #10
Hardware name: Freescale i.MX6 Quad/DualLite (Device Tree)
[<c01109f8>] (unwind_backtrace) from [<c010bad8>] (show_stack+0x10/0x14)
[<c010bad8>] (show_stack) from [<c0bf8c4c>] (dump_stack+0x84/0xc4)
[<c0bf8c4c>] (dump_stack) from [<c0c017e8>] (mutex_lock_nested+0x2c/0x4e4)
unwind: Unknown symbol address c01014d8
unwind: Index not found c01014d8
[<c0c017e8>] (mutex_lock_nested) from [<c0865cec>] (of_alias_get_id+0x20/0x78)
[<c0865cec>] (of_alias_get_id) from [<c07b5264>] (mmc_alloc_host+0x48/0x238)
[<c07b5264>] (mmc_alloc_host) from [<c07c5aa0>] (sdhci_alloc_host+0x1c/0x44)
[<c07c5aa0>] (sdhci_alloc_host) from [<c07cb1c8>] (sdhci_pltfm_init+0x58/0x1ec)
[<c07cb1c8>] (sdhci_pltfm_init) from [<c07cc980>] (sdhci_esdhc_imx_probe+0x30/0x724)
[<c07cc980>] (sdhci_esdhc_imx_probe) from [<c061ca00>] (platform_drv_probe+0x44/0xa8)
[<c061ca00>] (platform_drv_probe) from [<c061a8bc>] (driver_probe_device+0x198/0x2a8)
[<c061a8bc>] (driver_probe_device) from [<c061aaa4>] (__driver_attach+0x94/0x98)
[<c061aaa4>] (__driver_attach) from [<c0618d78>] (bus_for_each_dev+0x68/0x9c)
[<c0618d78>] (bus_for_each_dev) from [<c061a014>] (bus_add_driver+0x14c/0x1f4)
[<c061a014>] (bus_add_driver) from [<c061ba78>] (driver_register+0x78/0xf8)
[<c061ba78>] (driver_register) from [<c0101770>] (do_one_initcall+0x8c/0x1d8)
/soc/aips-bus@02100000/usdhc@02194000: voltage-ranges unspecified
sdhci-esdhc-imx 2194000.usdhc: Got CD GPIO
sdhci-esdhc-imx 2194000.usdhc: No vmmc regulator found
sdhci-esdhc-imx 2194000.usdhc: No vqmmc regulator found
unwind: Unknown symbol address c01014d8
unwind: Index not found c01014d8
mmc1: SDHCI controller on 2194000.usdhc [2194000.usdhc] using ADMA
unwind: Unknown symbol address c01014a4
unwind: Index not found c01014a4
unwind: Unknown symbol address c01014a4
unwind: Index not found c01014a4
unwind: Unknown symbol address c01014a4
unwind: Index not found c01014a4
unwind: Unknown symbol address c01014a4
unwind: Index not found c01014a4
unwind: Unknown symbol address c01014a4
unwind: Index not found c01014a4
unwind: Unknown symbol address c01014a4
unwind: Index not found c01014a4
unwind: Unknown symbol address c01014a4
unwind: Index not found c01014a4
/soc/aips-bus@02100000/usdhc@02198000: voltage-ranges unspecified
sdhci-esdhc-imx 2198000.usdhc: Got CD GPIO
sdhci-esdhc-imx 2198000.usdhc: No vmmc regulator found
sdhci-esdhc-imx 2198000.usdhc: No vqmmc regulator found
mmc2: SDHCI controller on 2198000.usdhc [2198000.usdhc] using ADMA
/soc/aips-bus@02100000/usdhc@0219c000: voltage-ranges unspecified
sdhci-esdhc-imx 219c000.usdhc: No vmmc regulator found
sdhci-esdhc-imx 219c000.usdhc: No vqmmc regulator found
unwind: Unknown symbol address c01014a4
unwind: Index not found c01014a4
unwind: Unknown symbol address c01014a4
unwind: Index not found c01014a4
unwind: Unknown symbol address c01014a4
unwind: Index not found c01014a4
unwind: Unknown symbol address c01014a4
unwind: Index not found c01014a4
unwind: Unknown symbol address c01014a4
unwind: Index not found c01014a4
mmc3: SDHCI controller on 219c000.usdhc [219c000.usdhc] using ADMA
mxc_vpu 2040000.vpu_fsl: VPU initialized
mxc_vdoa 21e4000.vdoa: i.MX Video Data Order Adapter(VDOA) driver probed
mxc_hdmi_cec soc:hdmi_cec@00120000: HDMI CEC initialized
Galcore version 5.0.11.41671
unwind: Unknown symbol address c01014a4
unwind: Index not found c01014a4
unwind: Unknown symbol address c01014a4
unwind: Index not found c01014a4
unwind: Unknown symbol address c01014a4
unwind: Index not found c01014a4
unwind: Unknown symbol address c01014a4
unwind: Index not found c01014a4
mmc2: host does not support reading read-only switch, assuming write-enable
mmc2: new high speed SDHC card at address aaaa
mmcblk2: mmc2:aaaa SD32G 29.7 GiB
unwind: Unknown symbol address c01014a4
unwind: Index not found c01014a4
unwind: Unknown symbol address c01014a4
unwind: Index not found c01014a4
mmcblk2: p1 p2 p3 < p5 > p4
mmcblk2: p4 size 57057280 extends beyond EOD, truncated
unwind: Unknown symbol address c01014a4
unwind: Index not found c01014a4
unwind: Unknown symbol address c01014a4
unwind: Index not found c01014a4
caam 2100000.caam: Entropy delay = 3200
caam 2100000.caam: Instantiated RNG4 SH0
caam 2100000.caam: Instantiated RNG4 SH1
caam 2100000.caam: device ID = 0x0a16010000000000 (Era -524)
caam 2100000.caam: job rings = 2, qi = 0
caam algorithms registered in /proc/crypto
unwind: Unknown symbol address c01014a4
unwind: Index not found c01014a4
unwind: Unknown symbol address c01014a4
unwind: Index not found c01014a4
unwind: Unknown symbol address c01014a4
unwind: Index not found c01014a4
unwind: Unknown symbol address c01014a4
unwind: Index not found c01014a4
unwind: Unknown symbol address c01014a4
unwind: Index not found c01014a4
caam_jr 2101000.jr0: registering rng-caam
platform caam_sm: blkkey_ex: 4 keystore units available
INFO: trying to register non-static key.
the code is fine but needs lockdep annotation.
turning off the locking correctness validator.
CPU: 0 PID: 1 Comm: swapper/0 Not tainted 4.1.15 #10
Hardware name: Freescale i.MX6 Quad/DualLite (Device Tree)
[<c01109f8>] (unwind_backtrace) from [<c010bad8>] (show_stack+0x10/0x14)
[<c010bad8>] (show_stack) from [<c0bf8c4c>] (dump_stack+0x84/0xc4)
[<c0bf8c4c>] (dump_stack) from [<c018ccd4>] (__lock_acquire+0x1cb4/0x2254)
[<c018ccd4>] (__lock_acquire) from [<c018dbd0>] (lock_acquire+0x118/0x36c)
[<c018dbd0>] (lock_acquire) from [<c0c06170>] (_raw_spin_lock+0x40/0x78)
[<c0c06170>] (_raw_spin_lock) from [<c0829fcc>] (sm_keystore_slot_alloc+0x24/0x74)
[<c0829fcc>] (sm_keystore_slot_alloc) from [<c082b098>] (caam_sm_example_init+0x1ec/0xb68)
[<c082b098>] (caam_sm_example_init) from [<c115cf8c>] (caam_sm_test_init+0x50/0x58)
[<c115cf8c>] (caam_sm_test_init) from [<c0101770>] (do_one_initcall+0x8c/0x1d8)
platform caam_sm: 64-bit clear key:
platform caam_sm: [0000] 00 01 02 03 04 0f 06 07
platform caam_sm: 64-bit black key:
platform caam_sm: [0000] 01 2a eb b3 3a 5f d7 04
platform caam_sm: [0008] ce b1 f6 17 b9 50 77 13
platform caam_sm: 128-bit clear key:
platform caam_sm: [0000] 00 01 02 03 04 0f 06 07
platform caam_sm: [0008] 08 09 0a 0b 0c 0d 0e 0f
platform caam_sm: 128-bit black key:
platform caam_sm: [0000] 50 67 17 50 f3 a1 5b 80
platform caam_sm: [0008] 0c 0d 77 68 78 63 82 6f
platform caam_sm: 192-bit clear key:
platform caam_sm: [0000] 00 01 02 03 04 0f 06 07
platform caam_sm: [0008] 08 09 0a 0b 0c 0d 0e 0f
platform caam_sm: [0016] 10 11 12 13 14 15 16 17
platform caam_sm: 192-bit black key:
platform caam_sm: [0000] 0a 8a a9 b7 6c fe 63 a9
platform caam_sm: [0008] 79 4e b4 40 14 2e bd 69
platform caam_sm: [0016] 5d 14 68 1b bb f3 8f 36
platform caam_sm: [0024] a6 6b 04 10 a4 7d 70 26
platform caam_sm: 256-bit clear key:
platform caam_sm: [0000] 00 01 02 03 04 0f 06 07
platform caam_sm: [0008] 08 09 0a 0b 0c 0d 0e 0f
platform caam_sm: [0016] 10 11 12 13 14 15 16 17
platform caam_sm: [0024] 18 19 1a 1b 1c 1d 1e 1f
platform caam_sm: 256-bit black key:
platform caam_sm: [0000] b7 e5 c1 84 66 e6 bd ce
platform caam_sm: [0008] 3f 45 ff 5f e9 d8 8a 55
platform caam_sm: [0016] 61 ca 81 86 41 06 d0 af
platform caam_sm: [0024] 98 d4 bb 4f 47 f1 d3 6f
platform caam_sm: 64-bit unwritten blob:
platform caam_sm: [0000] 00 00 00 00 00 00 00 00
platform caam_sm: [0008] 00 00 00 00 00 00 00 00
platform caam_sm: [0016] 00 00 00 00 00 00 00 00
platform caam_sm: [0024] 00 00 00 00 00 00 00 00
platform caam_sm: [0032] 00 00 00 00 00 00 00 00
platform caam_sm: [0040] 00 00 00 00 00 00 00 00
platform caam_sm: [0048] 00 00 00 00 00 00 00 00
platform caam_sm: [0056] 00 00 00 00 00 00 00 00
platform caam_sm: [0064] 00 00 00 00 00 00 00 00
platform caam_sm: [0072] 00 00 00 00 00 00 00 00
platform caam_sm: [0080] 00 00 00 00 00 00 00 00
platform caam_sm: [0088] 00 00 00 00 00 00 00 00
platform caam_sm: 128-bit unwritten blob:
platform caam_sm: [0000] 00 00 00 00 00 00 00 00
platform caam_sm: [0008] 00 00 00 00 00 00 00 00
platform caam_sm: [0016] 00 00 00 00 00 00 00 00
platform caam_sm: [0024] 00 00 00 00 00 00 00 00
platform caam_sm: [0032] 00 00 00 00 00 00 00 00
platform caam_sm: [0040] 00 00 00 00 00 00 00 00
platform caam_sm: [0048] 00 00 00 00 00 00 00 00
platform caam_sm: [0056] 00 00 00 00 00 00 00 00
platform caam_sm: [0064] 00 00 00 00 00 00 00 00
platform caam_sm: [0072] 00 00 00 00 00 00 00 00
platform caam_sm: [0080] 00 00 00 00 00 00 00 00
platform caam_sm: [0088] 00 00 00 00 00 00 00 00
platform caam_sm: 196-bit unwritten blob:
platform caam_sm: [0000] 00 00 00 00 00 00 00 00
platform caam_sm: [0008] 00 00 00 00 00 00 00 00
platform caam_sm: [0016] 00 00 00 00 00 00 00 00
platform caam_sm: [0024] 00 00 00 00 00 00 00 00
platform caam_sm: [0032] 00 00 00 00 00 00 00 00
platform caam_sm: [0040] 00 00 00 00 00 00 00 00
platform caam_sm: [0048] 00 00 00 00 00 00 00 00
platform caam_sm: [0056] 00 00 00 00 00 00 00 00
platform caam_sm: [0064] 00 00 00 00 00 00 00 00
platform caam_sm: [0072] 00 00 00 00 00 00 00 00
platform caam_sm: [0080] 00 00 00 00 00 00 00 00
platform caam_sm: [0088] 00 00 00 00 00 00 00 00
platform caam_sm: 256-bit unwritten blob:
platform caam_sm: [0000] 00 00 00 00 00 00 00 00
platform caam_sm: [0008] 00 00 00 00 00 00 00 00
platform caam_sm: [0016] 00 00 00 00 00 00 00 00
platform caam_sm: [0024] 00 00 00 00 00 00 00 00
platform caam_sm: [0032] 00 00 00 00 00 00 00 00
platform caam_sm: [0040] 00 00 00 00 00 00 00 00
platform caam_sm: [0048] 00 00 00 00 00 00 00 00
platform caam_sm: [0056] 00 00 00 00 00 00 00 00
platform caam_sm: [0064] 00 00 00 00 00 00 00 00
platform caam_sm: [0072] 00 00 00 00 00 00 00 00
platform caam_sm: [0080] 00 00 00 00 00 00 00 00
platform caam_sm: [0088] 00 00 00 00 00 00 00 00
platform caam_sm: 64-bit black key in blob:
platform caam_sm: [0000] d6 f7 00 d6 14 d5 3f ff
platform caam_sm: [0008] f3 9f 90 37 d1 b4 9b ab
platform caam_sm: [0016] c3 0c e4 c9 26 94 cf ee
platform caam_sm: [0024] f7 6a d4 22 7e ad bf 2d
platform caam_sm: [0032] 85 4b 95 7f 14 cd f8 e8
platform caam_sm: [0040] 9e f0 7a f2 71 dd 52 c6
platform caam_sm: [0048] 9b 65 c3 70 ba b3 7f 5b
platform caam_sm: [0056] 00 00 00 00 00 00 00 00
platform caam_sm: [0064] 00 00 00 00 00 00 00 00
platform caam_sm: [0072] 00 00 00 00 00 00 00 00
platform caam_sm: [0080] 00 00 00 00 00 00 00 00
platform caam_sm: [0088] 00 00 00 00 00 00 00 00
platform caam_sm: 128-bit black key in blob:
platform caam_sm: [0000] b7 61 8f d1 49 29 b8 c4
platform caam_sm: [0008] 54 2f 45 74 2c a8 43 3f
platform caam_sm: [0016] b5 fa dd 46 b3 cc e8 8e
platform caam_sm: [0024] c5 4c a5 d5 44 14 00 6e
platform caam_sm: [0032] 52 33 fa 13 69 0c 87 37
platform caam_sm: [0040] 80 cb de 42 19 18 6e a7
platform caam_sm: [0048] 3b e9 47 4c 98 a5 a1 7f
platform caam_sm: [0056] 24 ea 13 71 b7 6e f3 da
platform caam_sm: [0064] 00 00 00 00 00 00 00 00
platform caam_sm: [0072] 00 00 00 00 00 00 00 00
platform caam_sm: [0080] 00 00 00 00 00 00 00 00
platform caam_sm: [0088] 00 00 00 00 00 00 00 00
platform caam_sm: 192-bit black key in blob:
platform caam_sm: [0000] fa 33 37 ca c4 e5 3a 95
platform caam_sm: [0008] e0 18 7f 56 40 d0 10 e1
platform caam_sm: [0016] 97 ba 12 10 fc 0a d4 30
platform caam_sm: [0024] 44 46 f0 38 36 76 99 01
platform caam_sm: [0032] 7b 52 b2 62 2d c0 99 2c
platform caam_sm: [0040] 9c f7 7e b8 67 b7 65 1c
platform caam_sm: [0048] f0 fa d1 86 1b e5 d6 91
platform caam_sm: [0056] 16 83 fd 6a 82 23 09 d0
platform caam_sm: [0064] 82 f7 bd 06 55 0d f1 76
platform caam_sm: [0072] 00 00 00 00 00 00 00 00
platform caam_sm: [0080] 00 00 00 00 00 00 00 00
platform caam_sm: [0088] 00 00 00 00 00 00 00 00
platform caam_sm: 256-bit black key in blob:
platform caam_sm: [0000] 82 52 5b bd d0 36 80 8b
platform caam_sm: [0008] e1 69 49 fa af c3 87 40
platform caam_sm: [0016] 6b bc 35 de cd 1b a5 60
platform caam_sm: [0024] 73 ef da cf 4a 53 70 57
platform caam_sm: [0032] 5f 4b 0f 8c 85 12 7b cd
platform caam_sm: [0040] c7 be 53 4f e2 84 d5 5c
platform caam_sm: [0048] 22 af c3 e2 00 5e a4 29
platform caam_sm: [0056] 1a a6 9a ee f4 d2 14 0f
platform caam_sm: [0064] 4b dc ba 91 32 a6 5f 39
platform caam_sm: [0072] 04 bb 4e 57 d1 05 40 8d
platform caam_sm: [0080] 00 00 00 00 00 00 00 00
platform caam_sm: [0088] 00 00 00 00 00 00 00 00
platform caam_sm: restored 64-bit black key:
platform caam_sm: [0000] c5 b7 e3 6c 17 96 31 5b
platform caam_sm: [0008] 5c d7 c2 2c 79 09 d6 fb
platform caam_sm: restored 128-bit black key:
platform caam_sm: [0000] 50 67 17 50 f3 a1 5b 80
platform caam_sm: [0008] 0c 0d 77 68 78 63 82 6f
platform caam_sm: restored 192-bit black key:
platform caam_sm: [0000] 0a 8a a9 b7 6c fe 63 a9
platform caam_sm: [0008] 79 4e b4 40 14 2e bd 69
platform caam_sm: [0016] 3c 2b fb 11 eb d4 a4 a5
platform caam_sm: [0024] b3 27 1e f5 51 58 f8 9d
platform caam_sm: restored 256-bit black key:
platform caam_sm: [0000] b7 e5 c1 84 66 e6 bd ce
platform caam_sm: [0008] 3f 45 ff 5f e9 d8 8a 55
platform caam_sm: [0016] 61 ca 81 86 41 06 d0 af
platform caam_sm: [0024] 98 d4 bb 4f 47 f1 d3 6f
snvs-secvio 20cc000.caam-snvs: can't get snvs clock
snvs-secvio 20cc000.caam-snvs: violation handlers armed - non-secure state
caam_keyblob caam_keyblob: caam keyblob initialized
hidraw: raw HID events driver (C) Jiri Kosina
usbcore: registered new interface driver usbhid
usbhid: USB HID core driver
ashmem: initialized
usbcore: registered new interface driver snd-usb-audio
fsl-asrc 2034000.asrc: driver registered
fsl-hdmi-dai soc:hdmi_audio@00120000: failed to probe. Load HDMI-video first.
fsl-hdmi-dai: probe of soc:hdmi_audio@00120000 failed with error -12
imx-wm8960 sound: failed to find codec platform device
imx-wm8960: probe of sound failed with error -22
imx-audio-hdmi sound-hdmi: initialize HDMI-audio failed. load HDMI-video first!
NET: Registered protocol family 26
u32 classifier
Actions configured
Netfilter messages via NETLINK v0.30.
nf_conntrack version 0.5.0 (16384 buckets, 65536 max)
ctnetlink v0.93: registering with nfnetlink.
xt_time: kernel timezone is -0000
ip_tables: (C) 2000-2006 Netfilter Core Team
arp_tables: (C) 2002 David S. Miller
Initializing XFRM netlink socket
NET: Registered protocol family 10
mip6: Mobile IPv6
ip6_tables: (C) 2000-2006 Netfilter Core Team
sit: IPv6 over IPv4 tunneling driver
NET: Registered protocol family 17
NET: Registered protocol family 15
can: controller area network core (rev 20120528 abi 9)
NET: Registered protocol family 29
can: raw protocol (rev 20120528)
can: broadcast manager protocol (rev 20120528 t)
can: netlink gateway (rev 20130117) max_hops=1
Bluetooth: RFCOMM TTY layer initialized
Bluetooth: RFCOMM socket layer initialized
Bluetooth: RFCOMM ver 1.11
Bluetooth: BNEP (Ethernet Emulation) ver 1.3
Bluetooth: BNEP filters: protocol multicast
Bluetooth: BNEP socket layer initialized
Bluetooth: HIDP (Human Interface Emulation) ver 1.2
Bluetooth: HIDP socket layer initialized
8021q: 802.1Q VLAN Support v1.8
Key type dns_resolver registered
hctosys: unable to open rtc device (rtc0)
can-3v3: disabling
wlreg_on: disabling
sensor-supply: disabling
wm8962-supply: disabling
usb_h1_vbus: disabling
usb_otg_vbus: disabling
ALSA device list:
No soundcards found.
EXT3-fs (mmcblk2p5): error: couldn't mount because of unsupported optional features (240)
EXT2-fs (mmcblk2p5): error: couldn't mount because of unsupported optional features (244)
EXT4-fs (mmcblk2p5): recovery complete
EXT4-fs (mmcblk2p5): mounted filesystem with ordered data mode. Opts: (null)
VFS: Mounted root (ext4 filesystem) on device 179:5.
devtmpfs: mounted
Freeing unused kernel memory: 2048K (c1100000 - c1300000)
mkdir: can't create directory '/mnt/disk': File exists
grep: /etc/mtab: No such file or directory
fec 2188000.ethernet eth0: Freescale FEC PHY driver [Micrel KSZ9031 Gigabit PHY] (mii_bus:phy_addr=2188000.ethernet:03, irq=-1)
IPv6: ADDRCONF(NETDEV_UP): eth0: link is not ready

Please press Enter to activate this console. fec 2188000.ethernet eth0: Link is Up - 1Gbps/Full - flow control off
IPv6: ADDRCONF(NETDEV_CHANGE): eth0: link becomes ready
random: nonblocking pool is initialized

0 Kudos
Reply
2 Replies

2,262 Views
Zhiming_Liu
NXP TechSupport
NXP TechSupport

Hi

Can you use uart on uboot console? If yes, the kernel should not have issue, you may need to check the rootfs setting about console.

Best Regards
Zhiming

0 Kudos
Reply

2,326 Views
hexiaojun3
Contributor II

BTW: I have no "hwclock -w" process hooked issue.

0 Kudos
Reply