Kernel run failure in imx-p9.0.0_2.3.0

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Kernel run failure in imx-p9.0.0_2.3.0

912 Views
yibo_li
Contributor I

Hi, I built the version of imx-p9.0.0_2.3.0, download into mainboard

Expected result: uboot and kernel can boot success,

Actual result: uboot boot success, kernel boot failure, look from log, no return in gpu_init.

Compare with the demo version, the version is 'p9.0.0_2.0.1-ga',I observed the result as same as 'imx-p9.0.0_2.3.0'.

(Because I found that the latest demo version is 'p9.0.0_2.0.1-ga', so I used this version to verify in mainboard,  The attachment log is test for 'p9.0.0_2.0.1-ga', please refer to the attachment log.)

Thanks

Yibo

0 Kudos
Reply
3 Replies

689 Views
igorpadykov
NXP Employee
NXP Employee

Hi Yibo

 imx-p9.0.0_2.3.0 does not support i.MX8QM according to Release Notes

(attached) p.1 from Android P9.0.0_2.3.0 Documentation

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

689 Views
yibo_li
Contributor I

Hi Igor,

         Thanks your reply!

         Dose android_p9.0.0_1.0.0 support i.MX8QM?Which version can support  i.MX8QM?

         I debug in android_p9.0.0_1.0.0, also observed kernel boot failure.

Thanks

Yibo

         

0 Kudos
Reply

689 Views
igorpadykov
NXP Employee
NXP Employee

Hi Yibo

please check Android documentation (Release Notes p.1) on below link,

it shows supported platforms.

i.MX Software | NXP 

android_p9.0.0_1.0.0 supports i.MX8QM, please verify that your board is

i.MX 8QuadMax MEK Rev. B0 and apply all updates "i.MX BSP Updates and Releases "

on link i.MX Software | NXP 

like Android P9.0.0_1.0.4 Patch.

Best regards
igor

0 Kudos
Reply