Kernel panic when disabling usb gadget

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Kernel panic when disabling usb gadget

4,980件の閲覧回数
chris_f
Contributor V

I'm using kernel 4.9.88 on an iMX6ULL.

Sometimes, when disabling the usb gadget (by echo "" > UDC) the module locks completely.

I found this patch from @PeterChen for kernel 5.4:

https://patches.linaro.org/patch/223191/

and note that a similar problem was reported for kernel 4.4 (though patch was rejected) so assume it's the same issue in 4.9:

https://www.spinics.net/lists/linux-usb/msg159075.html

Could someone advise how to back-port Peter's patch to 4.9.88?

I can see what needs applying to udc/core.c but can't see yet where the usb_gadget structure is created so I can add the irq member.

0 件の賞賛
返信
4 返答(返信)

4,894件の閲覧回数
chris_f
Contributor V

I've now found the cause of the problem (the patch from @PeterChen isn't relevant).

It is not a kernel panic, it's a kernel lock up in the ChipIdea udc driver.

The function hw_ep_flush never returns. It is waiting for the hardware to complete endpoint flush that never happens.

https://elixir.bootlin.com/linux/latest/source/drivers/usb/chipidea/udc.c#L101

I've fixed this lock up by simply adding a timeout to that loop. If the flush doesn't complete we just continue as if it had. The next connection still works.

Further testing shows that there are other lock conditions that can occur (approx 1 in 200 connections) during connection/disconnection. There are a number of other loops in that code that will not exit unless the hardware complies.

I don't know if this hardware problem exists in other implementations using the ChipIdea driver but I can recreate it on multiple boards.

0 件の賞賛
返信

4,956件の閲覧回数
chris_f
Contributor V

Thanks Zhiming but I can't see where the new member gadget.irq is set?

There's a struct fsl_udc in fsl_udc_core which also has an irq member (and a gadget struct). That is set with platform_get_irq in fsl_udc_probe.

The patch creates a new member gadget.irq but it's never set?

0 件の賞賛
返信

4,924件の閲覧回数
Zhiming_Liu
NXP TechSupport
NXP TechSupport

Hi

 

Yes, I saw the source code and it isn't used in fsl_udc_remove. 

0 件の賞賛
返信

4,960件の閲覧回数
Zhiming_Liu
NXP TechSupport
NXP TechSupport

Hi

 

As patch shows,the gadget  is in 

/include/linux/usb/gadget.h

 

BR

Zhiming

タグ(1)
0 件の賞賛
返信