Dear sir.
our BSP is 5.0, kernel is 3.10.53 ,uboot 2014.04 and soc is imx6qsabresd 800MHz pmic is DA9063.
if Add PMIC driver ONEKEY Support. when power down,we get below info,and the machine will restart.
SysRq : Emergency Remount R/O
EXT4-fs (mmcblk3p4): re-mounted. Opts: (null)
EXT4-fs (mmcblk3p6): re-mounted. Opts: (null)
Emergency Remount complete
imx2-wdt 20c0000.wdog: Device shutdown: Expect reboot!
Power down.
Kernel panic - not syncing: Attempted to kill init! exitcode=0x00000000
and if remove ONEKEY support ,can't see this issue,but can't shutdown the power only shutdown android os.
how to fix this issue?
thanks all.
Hi li
I would suggest to check if hardware can trigger PMIC reset,
as described in Table 19. Known Issues and Workarounds
attached document.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------