hi,
I am working on imx6qp sabre auto board, (MCIMXABASEV1,MCIMX6QPAICPU3 cards).
building Linux ivi-image with yocto platform. it was working fine with Jethro realease.
but I wanted to move the Weston to latest version i.e Weston_1.11.0 build successful(except for Weston_1.13.0) but Weston was launching on target . so decided to move the yocto version to morty.
now yocto morty (repo init -u git://git.freescale.com/imx/fsl-arm-yocto-bsp.git -b imx-morty)
tried building image using : bitbake fsl-qt5-image -k.
here Linux-imx_4.9.11 as well as Linux-imx_4.1.15 not working ("fetcher failure errors")
so used Linux-imx_4.1.15.bb from jethro yocto build file .
kernel boot stops after "starting kernel " print.
is that correct?? let me know what to do? but still kernel not booting so copied kernel image from jethro build to sd-card and tried to check GUI here Weston not launching. please help here
this version has Weston_1.11.0. here also yocto build successful but when I try to launch the Weston I am getting segmentation fault. :smileysad: issue is same as with the yocto jethro version.
Please help me resolving this issue.
Note : please check the attachments.
Regards,
Lavakumar S